Deep Sleep |Zigbee 3.0|JN-SW-4170|JN-AN-1229|JN5168-001-M00

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Deep Sleep |Zigbee 3.0|JN-SW-4170|JN-AN-1229|JN5168-001-M00

1,183 Views
davidashraf
Contributor V

I want to try Deep Sleep option instead of SLEEP_OSCON_RAMON . When I try, the jn5168 module seems to sleep before doing its task.
Is there an example or application note using Deep Sleep ? 
Thanks.

0 Kudos
4 Replies

538 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi David,

Please take a look the JN516x Integrated Peripherals API User Guide

http://www.nxp.com/documents/user_manual/JN-UG-3087.pdf?fsrch=1&sr=1&pageNum=2 

3.2.3 Low-Power Modes

API: void vAHI_Sleep(teAHI_SleepMode sSleepMode);

Hope it helps.

Best Regards,

Mario

0 Kudos

538 Views
davidashraf
Contributor V

Any Idea yet ? 

0 Kudos

538 Views
davidashraf
Contributor V

Hi Mario , 
Is there a problem in using Power manager  ?
and Doesn't using vAHI_Sleep(teAHI_SleepMode sSleepMode) contradict with the mode initialized in " PWRM_vInit " ?

Thanks for your reply ? 

0 Kudos

538 Views
davidashraf
Contributor V

Any Ideas to solve this problem ? 

0 Kudos