Trying to get an AW-CM 358 m.2 radio module to work with an imx8mp evk board running Linux.
What configuration changes are needed to get the radio module to come up?
After swapping the module that comes with the evk for the AW-CM358 m.2 module, the radio is not coming up.
Just to make sure it was not our sw changes, I loaded the board with LF_v5.10.72-2.2.0_images_IMX8MPEVK.zip but the radio module is not being seen.
Thank you,
Amber
Solved! Go to Solution.
I was finally able to get the AW-CM358MA module to work by modifying the device tree to enable SDIO and disable pcie.
For anyone else that runs into this issue. The DTB blob that worked for me is imx8mp-evk-usdhc1-m2.dtb.
Are there changes needed to the device tree for the imx8mp in order to use the AW-CM358MA radio module?
Hello @amberworth,
If you're using the image in the following link you shouldn't need any change to the device tree and the other extra steps would be enable the SDIO interface as it mention in the 3.5 88W8987-based AzureWave AW-CM358MA module section in the app note that I previously mention.
BR,
Alexis Andalon
I was finally able to get the AW-CM358MA module to work by modifying the device tree to enable SDIO and disable pcie.
For anyone else that runs into this issue. The DTB blob that worked for me is imx8mp-evk-usdhc1-m2.dtb.
Hello @amberworth,
I will suggest to check the following two applications notes:
These two application notes describe how to set the driver and enable the module and its different features.
BR,
Alexis Andalon