Can KW2x support ZigBee 868 MHz?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can KW2x support ZigBee 868 MHz?

1,566 Views
benjaminchang
Contributor V

NXP KW2x is supporting 802.15.4, one of our customer is requesting ZigBee 2.4 GHz and 868 MHz (a GB requirement) since last year. So we proposed KW01Z + KW20Z to them. Checking the new EE Times in Feb., link:

http://electronicdesign.com/blog/multiprotocol-wireless-soc-targets-iot-connectivity?NL=ED-001&Issue...

We find there is a SiLabs’s Might Gecko wireless SoC supports “The SoC would normally be sleeping, but could periodically wake up to handle 802.15.4 Thread communication and then sub GHz communication

Why can SiLabs’s SoC support this dual-band communication, but KWxx chips cannot? Is this a H/W limitation or S/W issue?

Labels (2)
0 Kudos
Reply
1 Reply

712 Views
jc_pacheco
NXP Employee
NXP Employee

KW2xD - 2.4GHz radio

KW20/1Z - 2.4GHz radio

KW01Z - <1 GHz radio

0 Kudos
Reply