Do either of the following have CE Certification ?
CLRC66303
HTRC110
Thanks in advance.
Hi James,
Actually CE is for a complete product, not for a single IC like CLRC66303 or HTRC110.
Hope that makes sense,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------