Burst signal off cmd

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Burst signal off cmd

1,664件の閲覧回数
Peter17
Contributor I

we are running CE DFS test.

for adaptive COT test, we need to issue wifi burst signal command, then will pass the test case.

Is there any burst signal off command for nxp wifi?

thanks

ラベル(3)
0 件の賞賛
返信
8 返答(返信)

1,615件の閲覧回数
nxf89619
NXP TechSupport
NXP TechSupport

Most of the information related to this process is under "Secure Files" on the page of each NXP device.
The process to retrieve this information is

  1. Go to the desired NXP device (for example, 88W9098)
  2. Scroll down to "Documentation"
  3. Select "Secure Files"
  4. Search for "DFS AN" or "DFS Application Note"

If you have any questions, please, feel free to ask.

0 件の賞賛
返信

1,609件の閲覧回数
Peter17
Contributor I

Hi AlanRadirez,
I can not find the document/website.
Could you please tell me the website address or document name?

or attach it to this forum?

Thanks

0 件の賞賛
返信

1,595件の閲覧回数
nxf89619
NXP TechSupport
NXP TechSupport

I cannot provide the file directly or a link to it because it is under a NDA, however, I can provide a guide to get the file.

In https://nxp.com under "My Account" there is a button called "Secure Files"

Secure Files button.png

 

 

 

 

And then select "Files" and search for DFS

Search files.png

 

 

 

0 件の賞賛
返信

1,577件の閲覧回数
Peter17
Contributor I

Hi AlanRamirez,

I have found DFS AN, but there is no Burst signal off command information.

We need the command to let burst signal off in order to pass COT test.

Please help to provide the command.

Thanks

0 件の賞賛
返信

1,551件の閲覧回数
Matt3
Contributor I

Based on my experience, and feedback from the lab, other vendors issue burst off command when running the COT test. 
Is there similar command from NXP chipset?

 

0 件の賞賛
返信

1,510件の閲覧回数
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Please check the Zero Wait AN for the 88w9098/88Q9098 in the same way that you searched for the first application note

 

Regards

0 件の賞賛
返信

1,625件の閲覧回数
Matt3
Contributor I

Does it need to run additional commands in order to pass the COT test?

What are the commands?

0 件の賞賛
返信

1,643件の閲覧回数
Peter17
Contributor I

The related information as below:
FW: pcieuart9098_combo_v1.bin
Driver: PCIE9098--17.68.1.p109.2-MXM5X17312.p5-GPL-(FP68)

0 件の賞賛
返信