Burst signal off cmd

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Burst signal off cmd

1,676 次查看
Peter17
Contributor I

we are running CE DFS test.

for adaptive COT test, we need to issue wifi burst signal command, then will pass the test case.

Is there any burst signal off command for nxp wifi?

thanks

0 项奖励
回复
8 回复数

1,627 次查看
nxf89619
NXP TechSupport
NXP TechSupport

Most of the information related to this process is under "Secure Files" on the page of each NXP device.
The process to retrieve this information is

  1. Go to the desired NXP device (for example, 88W9098)
  2. Scroll down to "Documentation"
  3. Select "Secure Files"
  4. Search for "DFS AN" or "DFS Application Note"

If you have any questions, please, feel free to ask.

0 项奖励
回复

1,621 次查看
Peter17
Contributor I

Hi AlanRadirez,
I can not find the document/website.
Could you please tell me the website address or document name?

or attach it to this forum?

Thanks

0 项奖励
回复

1,607 次查看
nxf89619
NXP TechSupport
NXP TechSupport

I cannot provide the file directly or a link to it because it is under a NDA, however, I can provide a guide to get the file.

In https://nxp.com under "My Account" there is a button called "Secure Files"

Secure Files button.png

 

 

 

 

And then select "Files" and search for DFS

Search files.png

 

 

 

0 项奖励
回复

1,589 次查看
Peter17
Contributor I

Hi AlanRamirez,

I have found DFS AN, but there is no Burst signal off command information.

We need the command to let burst signal off in order to pass COT test.

Please help to provide the command.

Thanks

0 项奖励
回复

1,563 次查看
Matt3
Contributor I

Based on my experience, and feedback from the lab, other vendors issue burst off command when running the COT test. 
Is there similar command from NXP chipset?

 

0 项奖励
回复

1,522 次查看
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Please check the Zero Wait AN for the 88w9098/88Q9098 in the same way that you searched for the first application note

 

Regards

0 项奖励
回复

1,637 次查看
Matt3
Contributor I

Does it need to run additional commands in order to pass the COT test?

What are the commands?

0 项奖励
回复

1,655 次查看
Peter17
Contributor I

The related information as below:
FW: pcieuart9098_combo_v1.bin
Driver: PCIE9098--17.68.1.p109.2-MXM5X17312.p5-GPL-(FP68)

0 项奖励
回复