Hello, NXP community.
We are working on Bluetooth 5 LE extended advertising using BT module based-on 88W909/88Q09098 chip. We recognized that he module supports all Bluetooth 5 LE extended features in a document we received.
I brought up the module on our system and It worked well about BLE advertising.
But we want to use BLE extended advertising.
I used following HCI commands to receive BLE extended advertising.
However, btmon app cannot receive any extended advertising beacon from our test smartphone.
How should we send the set of HCI commands for tesing the BT module to receive extended advertising beacons?
Is there any test example for Bluetooth5 extended advertising using 88X9098 chip ?
Hi @ytpark,
Here one step is missing while configuring the set event mask. As provided logs having only LE Set Event Mask but not the overall Set Event Mask.
#Set Event Mask
sudo hcitool -i hci1 cmd 0x03 0x0001 ff ff ff ff ff ff ff 3f
sudo hcitool -i hci1 cmd 0x03 0x0003
#Set Event Mask
sudo hcitool -i hci1 cmd 0x03 0x0001 ff ff ff ff ff ff ff 3f
#set LE Set Event mask
sudo hcitool -i hci1 cmd 0x08 0x0001 ff ff ff ff ff ff ff ff
#Set Default PHY
sudo hcitool -i hci1 cmd 0x08 0x0031 0x00 0x04 0x04
#LE set extended scan parameters
sudo hcitool -i hci1 cmd 0x08 0x0041 00 00 01 01 30 00 30 00
sleep 1
#LE set extended scan enable
sudo hcitool -i hci1 cmd 0x08 0x0042 01 00 00 00 00 00
sleep 30
Regards,
Mario