Hi all,
I am trying to program USB-KW38 / FRDM-KW38 using MCU Expresso IDE for my Beacon Project. I would be helpful if someone could direct me to obtain the sample codes for the following in reference to USB-KW38 / FRDM-KW38:
I could find a beacon example inside SDK examples for FRDM-KW38, but couldn't find any for the others.
Please do share any pointers for the following too:
Thanks in advance
Hi Vidya, I hope you're doing well!
The FRDM-KW38 SDK examples which could be useful for implementing a Beacon or a Scanner:
Regarding programming the devices using Python, it is possible to use the Host-SDK included in the KW38's SDK to program the device using Linux with FSCI commands. More information about this can be found in the following path:
<…\SDK_2.6.6_FRDM-KW38\tools\wireless\host_sdk\hsdk\doc>
And in the Connectivity Framework Reference Manual, chapter 3.11, included in the SDK's Documentation Package:
<…\SDK_2.6.6_FRDM-KW38_doc\docs\wireless\Common\Connectivity Framework Reference Manual.pdf>
And last but not least, all of the currently available example codes for the RDDRONE-8MMNavQ can be found on our Gitbook page.
Please let me know if you need any more information.
Best regards,
Sebastian