Hi, all.
As BGU8007, BGU8009 and BGU8103 has ENABLE pin.
ENABLE=Low means OFF state according to the datasheet.
Does output become to Hi-Z when OFF state?
best regards,
tomo
When device is disabled, the internal transistor biasing is turned off and device doesn't consume supply power.
Note. Output is AC coupled. AC impedance is not HiZ when device is disabled.
Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------