AFT05MP075

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AFT05MP075

673 Views
yunwang666
Contributor I

I use ADS simulated AFT05MP075 results is not like the datasheet Figure 3 Drain current verse Drain-Source Voltage,I want to know if it is a datasheet error or simulation error.

0 Kudos
1 Reply

653 Views
LPP
NXP Employee
NXP Employee

AFT05MP075 ADS model has been optimized to match measured RF performance.

DC parameter was not specially tuned. In fact, most of the difference between datasheet Figure 3 and simulation is determined by different gate threshold voltages of the model and of the datasheet instance. This value is about 0.5V more in the model vs datasheet sample.

Note 1. Gate threshold voltage can differ from sample to sample due to production spread. Datasheet specifies VGS(th)=[1.7,2.5]V. Figure 3 was measured on the device with VGS(th)~2V whereas the threshold in the model is closer to 2.5V.

Note 2. The accuracy of DC model is not critical, since the gate bias voltage of each device has to be tuned individually.

Have a great day,
Pavel
TIC

 

0 Kudos