88w8987 bt class 2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

88w8987 bt class 2

1,033 次查看
eric_delanghe
Contributor II

Hello,

I'm trying to update bt power class of the 88w8987 and I haven't succeed yet.

Their is no information in the datasheet and labtool is still failing.

What can I do ?

Best,

Eric Delanghe

eric.delanghe@faurecia.com

btmon log
@ RAW Open: labtool (privileged) version 2.22                               {0x0004} [hci1] 1086.933839
< HCI Command: Vendor (0x3f|0x0200) plen 16                                     #246 [hci1] 1091.805552
        10 20 00 00 00 00 00 00 00 00 00 00 00 00 00 00  . ..............
> HCI Event: Command Complete (0x0e) plen 4                                     #247 [hci1] 1091.817983
      Vendor (0x3f|0x0200) ncmd 1
        Status: Unknown HCI Command (0x01)
< HCI Command: Vendor (0x3f|0x0200) plen 16                                     #248 [hci1] 1098.893864
        10 20 00 00 01 00 00 00 00 00 00 00 01 00 00 00  . ..............
> HCI Event: Command Complete (0x0e) plen 4                                     #249 [hci1] 1098.904827
      Vendor (0x3f|0x0200) ncmd 1
        Status: Unknown HCI Command (0x01)
< HCI Command: Vendor (0x3f|0x0200) plen 16                                     #250 [hci1] 1100.869452
        10 20 00 00 00 00 00 00 00 00 00 00 00 00 00 00  . ..............
> HCI Event: Command Complete (0x0e) plen 4                                     #251 [hci1] 1100.883948
      Vendor (0x3f|0x0200) ncmd 1
        Status: Unknown HCI Command (0x01)
@ RAW Close: labtool                                                        {0x0004} [hci1] 1107.677318

Labtool logs
Name:        Dut labtool
Version:    1.0.0.146
Date:        Jan 20 2020 (14:54:03)

Note:        

1. =========WiFi tool=============
2. =========BT   tool=============

Enter CMD 99 to Exit

Enter option: 2
Name:        DutApiClass
Interface:    Version:    1.0.0.146
Date:        Jan 20 2020 (14:54:03)

Note:        

Initialize drvwrapper for BT ....
 Dut_Bt_OpenDevice: 0x00000000
-----------------------------------------------------------------------
        W87xx (BT) TEST MENU
-----------------------------------------------------------------------
Enter option: 113
113

 Dut_Bt_GetBtPwrControlClass: 0x00000001
 Power Control Class Mode 0
Enter option: 114 1
114 1

 Dut_Bt_SetBtPwrControlClass: 0x00000001
Enter option: 113
113

 Dut_Bt_GetBtPwrControlClass: 0x00000001
 Power Control Class Mode 0
Enter option: 99
99

Exiting
De-Initialize drvwrapper for BT....
1. =========WiFi tool=============
2. =========BT   tool=============

Enter CMD 99 to Exit

Enter option: 99
Exiting
标记 (4)
0 项奖励
回复
1 回复

924 次查看
zhay
NXP Employee
NXP Employee

Dear customer, 

Which SW release package you're using? Is it MFG fw, or production fw? Cause the production fw doesn't support labtool at all. Also please share the driver/fw loading logs(dmesg) to check if they're loaded successfully.

Thanks,

Ying

0 项奖励
回复