802.15.4 radio: impedance matching and 3rd harmonic filter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

802.15.4 radio: impedance matching and 3rd harmonic filter

1,383 Views
AlanCollins
Contributor V

All our reference HW designs for 802.15.4 platforms have extra passive components (capacitors and inductors) near to the printed F antenna. 

  The ~0.5pF C and ~8.2nH L components are used for 3rd harmonic tests. This filter is needed for resonance the 3rd harmonic. However you might use the footprint to implement your own filter for personal tests.

            These components are not required for the common transceiver usage. You may not put those components for your design. Please notice that ~10pF Cmust be in your design because it is used for suppressing DC signals.

I do not recommend using a jumper or switch to change from PCB to external antenna and vice-versa (also applies for chip antennas). Either the jumper or switch will bring extra impedance and noise to the system. Then the antenna will not work as good as it should (decreasing the dBm capabilities). A Zero-ohm resistor can be used as a “wire link”. If you want to use the external antenna, you need to change the zero-ohm resistor.

Theoretically you won't have any loses using a zero-ohm resistor, but we know that nothing is perfect in the real world. The loses you will have depends on the resistor quality (depends on the materials, fabricator, etc). Unfortunately, we have not characterized the resistor loses in dBm. Our ZigBee hardware expert recommends that you may use a 10pF capacitor instead of a Zero ohm resistor. The advantage on the capacitor is that when you are in soldering phase, the resistor material may get noise from the process and generate a different ohms characteristic, while the capacitor will not have any problem. However any of the two possibilities will work well for your design.

Please feel free to add more information about impedance matching and similar topics.

Labels (1)
Tags (1)
3 Replies

1,031 Views
Antonio_Quiroz
NXP Employee
NXP Employee

Adding some comments to the post, for 802.15.4 devices also provide some Reference Document and Application Notes for RF Evaluation, Test Guidelines and Hardware Considerations, for solid RF design with 802.15.4 radios.

- AN4957 - HW Design Considerations for MKW2x devices

- ZHDCRM - Zigbee Package and HW Layout Considerations

- ZRFETRM - RF evaluation and Test Guidelines

- AN2731 - Antennas, Design and Aplications for 802.15.4 devices

1,031 Views
Wilgaced
Contributor II

Hi A_quiroz

     A gerber files for AN4957 i am loking for it but i can't find it.

0 Kudos

1,031 Views
Antonio_Quiroz
NXP Employee
NXP Employee

Hello Wilkins,

For KW2x devices NXP has three different form factors that you can use as base line for any design, Tower System, Freedom and USB dongle, depends on your application and size constraints you can use any of those.

All of them you may find on our web page, attached you may find links.

USB-KW24

-     http://cache.nxp.com/files/32bit/hardware_tools/schematics/USB-KW24D512_PCBRD.zip

FRDM-KW24

-     https://www.nxp.com/webapp/Download?colCode=FRDM-KW24D512-DESIGN-FILES&location=null&Parent_nodeId=1...

TWR-KW24

-     http://cache.nxp.com/files/32bit/hardware_tools/schematics/TWR-KW24D512_PCBRD.zip

I hope this may be helpful.

Regards,

Antonio Q

0 Kudos