无线连接知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Wireless Connectivity Knowledge Base

讨论

排序依据:
Document Purpose This post entry provides an example of a hybrid application (Wireless_UART + GFSK Advertising) by covering Bluetooth Low Energy multiple node connections in parallel with GFSK (Generic Frequency Shift Keying) communication.  This is an additional example for the SDK where we have defined a Hybrid application for Bluetooth LE advertising and scanning in parallel with GFSK communication. Audience The goal of this post is to serve as a guide for software developers who want to use, adapt and integrate GFSK functionality in a Bluetooth Low Energy application.    Setting up the development environment Toolchain:           - IAR Embedded Workbench 8.32 or newer;            https://www.iar.com/iar-embedded-workbench/   SDK:          - This version of firmware has been tested using SDK_2.2.1_FRDM-KW36, that can be downloaded using the following link: https://mcuxpresso.nxp.com/en/select            (please consider to select as Toolchain/IDE: All toolchains);             Hardware:       - 2 to 5 FRDM-KW36 development board:  FRDM-KW36 Development Kit KW36/35 MCUs | NXP  Implementation This demo application is design for the FRDM-KW36 platform and can be easily integrated into any board that is using KW35/36 MCU family. The functionality is based on the coexistence mechanism available on the SDK (Mobile Wireless System - MWS module). Based on the HW link-layer implementation, the Bluetooth Low Energy has a higher priority than the GFSK protocol and as the effect, the GFSK communication is executed during the Idle states (inactive periods) of the Bluetooth LE.  For more details related to the MWS module, please refer to connectivity framework documentation from SDK (Connectivity Framework Reference Manual.pdf). As for functionality on the Bluetooth low energy, both roles, central and peripheral, are supported.  Integration to the KW36 SDK - download the attached file and unzip to ...\SDK_2.2.1_FRDM-KW36\boards\frdmkw36\wireless_examples\hybrid folder: - open IAR project (SDK_2.2.1_FRDM-KW36_2019_07_19\boards\frdmkw36\wireless_examples\hybrid\ble_w_uart_gfsk\freertos\iar\ble_w_uart_gfsk_freertos.eww). - the project is organized like below: Functionality Switches functionality:     - functionality is defined in main.c file, BleApp_Handle Keys function;    - on the FRDM-KW36 we have:                 - SW2 - start scanning - Central device;                 - Long SW2 - start advertising - Peripheral device; (long SW2 - SW2 pressed for more than 3 seconds)                 - SW3 - start/stop GFSK TX operation (advertising);                 - Long SW3 - start/stop GFSK RX operation (long SW3 - SW3 pressed for more than 3 seconds) Logs:    - Serial events for different states of the board;    - BaudRate 115200; Validation The solution has been validated using 1 Master and 4 Slave devices as below: 1. Create the network:     a. Open serial communication of all devices. After reset you will see the following message:    b. On the Central device press SW2 to start scanning;    c. On the Peripheral device press Long SW2 to start advertising and wait for the confirmation on the serial port:   d. Repeat steps b. and c. for all of the slave devices.   e. When the network is completed on the Central device you will see something like below:   f. Check the over the air connections (connection interval = 312.5 ms): 2. Validate functionality on the Bluetooth LE: - from each slave (Peripheral) serial terminal write a message (e.g: testslaveX) and check that the message is printed on the master serial port. - do the same test from the master (Central) serial terminal. - Below is an example of this step:   - over the air log: 3. Initiate GFSK communication: - in one of the board's press SW3 to start GFSK TX operation (Advertising packet with AdvAddress = 0909090909); At every 1 second (gGenFskApp_TxInterval_c), an ADV packet will be sent over the air. - Select other board and press Long Sw3 to initiate GFSK RX operation (RX interval = 100ms = gGenFskApp_RxInterval_c); - Each time an ADV packet from address = 0909090909 is received this will be listed on the serial port as below: - over the air the GFSK TX packets will be listed as a ADV_NONCONN_IND: 4. Validate Bluetooth LE in parallel with GFSK: - write a message on the Master (Central) serial terminal and check the feedback on the slave(Peripheral) serial terminals: Attached is the source code for this application. Regards, Ovidiu
查看全文
With the release of the Bluetooth LE core erratum 10734, two new Host test cases (SM/SLA/KDU/BI-01-C and SM/MAS/KDU/BI-01-C) were added to the Test Case Reference List (TCRL) and are active since 24-Jan-19. This has an impact on new product qualifications based on Component (Tested) QDIDs that used an older TCRL when the test cases for this erratum were not required. Products that rely on NXP HOST QDIDs have 2 options for covering the erratum 10734 in order to complete the qualification: NXP provides a new qualification/QDID that includes these 2 tests. This is scheduled for later this year for QN908x, KW35/36 and KW41/31 products. NXP provides the test evidence/logs for these 2 tests and the test house reviews them before completing the product qualification. Right now, option 2 can be followed using the test evidence/logs provided by NXP. Later in the year, option 1 can be followed with an updated QDID. To obtain the test evidence/logs, please submit a support request.
查看全文
Regarding to the "Reprogramming a KW36 device using the OTAP Client Software" and "Reprogramming a KW35 device using the OTAP Client Software" documents, there are some additional steps to debug the OTAP client software in the specific case when you use MCUXpresso together with a P&E micro debug probe. Just before to program the OTAP client project (the second software), the user must do the following: Open the "Debug Configurations" view clicking on the green bug as depicted below. Go to the "Debugger" perspective and search the "Advanced Options" button. Enable the "Preserve this range (Memory Range 0)" checkbox, and edit the textbox "From: 0" To: 1fff" for the KW36 device or "From: 0 To: 3fff" for the KW35 device. After to flash the device, disconnect and connect again. If everything it's OK, the RGB LED must blink (If you are using an FRDM board). Then, test the demo as described in the document.
查看全文
This Application Note provides guidance on migrating ZigBee 3.0 Base device application designed for the NXP JN516x wireless microcontrollers to the KW41Z with the help of attached PDF.
查看全文
The FRDM-KW36 comes with the OpenSDA circuit which allows users to program and debug the evaluation board. There are different solutions to support such OpenSDA circuits: 1. The J-Link (SEGGER) firmware.  2. The CMSIS-DAP (mbed) firmware. The FRDM-KW36 comes pre-programmed with the CMSIS-DAP firmware. However, if you want to update the firmware version, you need to perform the next steps.  Press and hold the Reset button (SW1 push button in the board).  Unplug and plug the FRDM-KW36 again to the PC.  The board will be enumerated as "DAPLINKBOOT" device. Drag and drop the binary file to update the OpenSDA firmware.  If the J-Link version is programmed, the board will be enumerated as "FRDM-KW36J". On the other hand, if the CMSIS-DAP version is programmed, the board will be enumerated as "FRDM-KW36". The binary for the J-link version can be downloaded from the next link: SEGGER - The Embedded Experts - Downloads - J-Link / J-Trace  The binary for the CMSIS-DAP version can be found in the next link: OpenSDA Serial and Debug Adapter|NXP    Hope this helps... 
查看全文
I got a question related to best practices to configure a GPIO if the pin is not used. To make it short, the recommendation is to leave the GPIO floating on the PCB and leave the GPIO in its "Default" state as shown in the Signal Multiplexing table in the Reference Manual. The Default state is either “Disabled” or an analog function.   Some Kinetis devices have analog only pins (PGAx/ADCx) while most have GPIO pins with analog functions (PTx/ADCx) or digital GPIO pins   Unused pins, whether analog only or GPIO, should be left floating. Analog only pins do not have input buffers that will cause shoot-through currents when the input floats. GPIO pins with analog functions default to analog functions, which disables the digital input buffer – no shoot-through current.   The digital GPIO pins default to "Disabled", which disables the input buffers - no shoot-through currents with floating inputs.   Finally, unused pins shall not be tied to VDD or VSS. Hence, when designing your board and there are some unused pins, leave them floating on the PCB and then make sure that the software leaves the GPIO in its Default state in the MUX register. 
查看全文
This document describes the Persistent Data Manager (PDM) module which handles the storage of stack context data and application data in Non-Volatile Memory (NVM). For the KW41Z devices, this memory is internal Flash and this document will therefore refer to Flash. Tip: In this document, a cold start refers to either a first-time start or a re-start without memory (RAM) held. A warm start refers to a re-start with memory held (for example following sleep with memory held). 1.    Overview If the data needed for the operation of a network node is stored only in on-chip RAM, this data is maintained in memory only while the node is powered and will be lost during an interruption to the power supply (e.g. power failure or battery replacement). This data includes context data for the network stack and application data. In order for the node to recover from a power interruption with continuity of service, provision must be made for storing essential operational data in Non-Volatile Memory (NVM), such as Flash. This data can then be recovered during a re-boot following power loss, allowing the node to resume its role in the network. The storage and recovery of operational data in KW41Z Flash can be handled using the Persistent Data Manager (PDM) module, as described in the rest of this document, which covers the following topics: Initializing the PDM module - see Section 2 Managing data in Flash - see Section 3 PDM features like record searching by record ID – see Section 4 The PDM can be used with ZigBee PRO and IEEE802.15.4 wireless networking protocols. 2.    Initializing the PDM and Building a File System Using the Kinetis NVM framework requires that the user must register the necessary data sets for NVM writing. This is done by calling function NVM_RegisterDataSet(). This function registers the given data set to be written in the NVM_TABLE section from Flash. The PDM module must be initialized by the application following a cold or warm start, irrespective of the PDM functionality used (e.g. context data storage or counter implementation). PDM initialization is performed using the function PDM_eInitialise(). This function requires the following information to be specified: The number of Flash sectors to be used by PDM (a zero value means use all segments) Once the PDM_eInitialise() function has been called, the PDM module builds a file system in RAM containing information about the sectors that it manages in Flash. The PDM reads the header data from each Flash sector and builds the file system. Application records are grouped and initialized in function InitAplRecords(), while network stack records are grouped and initialized in function InitNwkRecords(). For ZigBee PRO, the PDM is used in its most general form, as described above. 3.    Managing Data in Flash This section describes use of the PDM module to persist data in Flash in order to provide continuity of service when the KW41Z device resumes operation after a cold start or a warm start without memory held. Data is stored in Flash in terms of ‘records’. A record occupies at least one Flash sector but may be larger than a sector and occupy multiple sectors. Any number of records of different lengths can be created, provided that they do not exceed the Flash capacity. The records are created automatically for stack context data and by the application (as indicated in Section 3.1) for application data. Each record is identified by a unique 16-bit value which is assigned when the record is created - for application data, this identifier is user-defined. The stack context data which is stored in Flash includes the following: Application layer data: AIB members, such as the EPID and ZDO state Group Address table Binding table Application key-pair descriptor Trust Centre device table Network layer data: NIB members, such as PAN ID and radio channel Neighbor table Network keys Address Map table On performing a KW41Z cold start or warm start without RAM held, the PDM must be initialized in the application as described in Section 2. If this is the first ever cold start, there will be no stack context data or application data preserved in the Flash. If it is a cold or warm start following previous use (such as after a reset), there should be stack context data and application data preserved in the Flash. On start-up, the PDM builds a file system in RAM and scans the Flash for valid data. If any data is found, it is incorporated in the file system. Saving and recovering application data in Flash are described in the subsections below. 3.1   Saving Data to Flash       Application data and stack context data are saved from RAM to Flash as described below.       Note: During a data save, if the Flash needs to be defragmented and purged, this will be performed automatically resulting in all records being re-saved.     Application data           You should save application data to Flash when important changes have been made to the data in RAM. Application data in RAM can be saved to an individual record           in Flash using the function PDM_eSaveRecordData(). A buffer of data in RAM is saved to a single record in Flash (a record may span multiple Flash sectors).          The records are created when calling PDM_eInitialise(). These records are traced by a unique 16-bit identifier assigned by the application - this identifier is subsequently          used to reference the record. The value used must not clash with those used by the NXP libraries - the ZigBee PRO stack libraries use values above 0x8000.          Subsequently, in performing a re-save to the same record (specified by its 16-bit identifier), the original Flash sectors associated with the record will be overwritten but          only the sector(s) containing data changes will be altered (if no data has changed, no write will be performed). This method of only making incremental saves improves          the occupancy level of the size-restricted Flash.     Stack Context Data          The NXP ZigBee PRO stack automatically saves its own context data from RAM to Flash when certain data items change. This data will not be encrypted. 3.2   Recovering Data from Flash       Application data and stack context data are loaded from the Flash to RAM as described below.     Application Data             During a cold start or a warm start without memory held, once the PDM module has been initialized (see Section 2.2), PDM_eReadDataFromRecord() must be called             for each record of application data in Flash that needs to be copied to RAM.     Stack Context Data             The function PDM_eReadDataFromRecord(), described above, is not used for records of stack context data. Loading this data from the Flash to RAM is handled             automatically by the stack (provided that the PDM has been initialized). 3.3   Deleting Data in Flash         All records (application data and stack context data) in the Flash can be deleted using the function PDM_vDeleteAllDataRecords().          Caution: You are not recommended to delete records of ZigBee PRO stack context data by calling PDM_vDeleteAllDataRecords() before a rejoin of the same secured          network. If these records are deleted, data sent by the node after the rejoin will be rejected by the destination node since the frame counter has been reset on the source          node. For more information and advice, refer to the “Application Design Notes” appendix in the ZigBee 3.0 Stack User Guide. 4.    PDM Features PDM offers a function that can be used to search for a specific record by using the 16-bit record ID. This function is called PDM_GetNVMTableEntry() and the required parameters are the record ID and an output pointer for the found entry. Another available PDM feature is providing a mechanism to safely write the data to NVM. This is done by calling the function PDM_vCompletePendingOperations(), which calls the appropriate NVM function that is used to complete all writings to NVM before any other operation. As an example, user can use this function to make sure that the data is written to the NVM before a reset.
查看全文
This post explains the implementation to operate the KW36 MCU on VLPR when the clocking mode is BLPE or BLPI. It's also included the explanation on how to configure clocks for BLPE and BLPI modes. For this example, the beacon demo from the wireless examples of the FRDM-KW36 is used. FRDM-KW36 SDK can be downloaded from MCUXpresso webpage. A recommended option to configure clock modes is "Config Tools" from MCUXpresso. Config Tools is embedded to MCUXpresso IDE, or you can download Config Tools from this LINK if you are using other supported IDE for this tool. MCUXpresso IDE is used in this example. Configure BLPE or BLPI clocking modes Select your proyect on MCUXpresso IDE, then open the clocks configuration window from Config Tools by clicking the arrow next to Config Tools icon from your MCUXpresso IDE, and then select "Open Clocks" as shown in Figure 1. Figure 1. Open Clocks from Config Tools using MCUXpresso IDE. A clocks diagram window will be opened. To configure the clock modes just select your option "BLPI" or "BLPE" on MCG Mode as shown in Figure 2. Clock will be automatically configured. Figure 2. MCG Mode selection. Now let's configure the appropiate clocks for Core clock and Bus clock to run in VLPR. Figure 3 taken from KW36 Reference Manual shows achievables frequencies when MCU is on VLPR.  Figure 3. VLPR clocks. Core clock should be 4MHz for BLPE and BLPI clocking modes, and Bus clock should be 1MHz for BLPE and 800kHz for BLPI.  Figure 4 shows clocks distribution for BLPE and Figure 5 for BLPI to operate with discussed frequencies. Figure 4. Clock distribution - VLPR and BLPE. Figure 5. Clock distribution - VLPR and BLPI. Press "Update Project" (Figure 6) to apply your new clock configuration to your firmware, then change perspective to "Develop" icon on right corner up to go to your project (See Figure 7). Compile your project to apply the changes. Figure 6. Update Project button. Figure 7. Develop button. At this point your project is ready to work with BLPE or BLPI clocks modes. Now, let's configure MCU to go to VLPR power mode. Configure VLPR mode VLPR mode can be configured using Config Tools too, but you may have an error trying to configure it when BLPE mode, this is because CLKDIV1 register cannot be written when the device is on VLPR mode. For this example, let's configure MCU into VLPR mode by firmware. Follow next steps to configure KW36 into VLPR power mode: 1. Configure RF Ref Oscillator to operate in VLPR mode. By default, the RF Ref Osc it's configured to operate into RUN mode. To change it to operate on VLPR mode just change the bits RF_OSC_EN from Radio System Control from 1 (RUN) to 7 (VLPR). Figure 8 taken from KW36 Reference Manual shows RF_OSC_EN value options from Radio System Control.    Figure 8. RF_OSC_EN bits from Radio System Control register. Go to clock_config.c file in your MCUXpresso project and search for "BOARD_RfOscInit" function. Change the code line as shown in Figure 9 to configure RF Ref Osc to work into VLPR mode. You may see a window asking if you want to make writable the read-only file, click Yes. Figure 9. Code line to configure RF Ref Osc to work into VLPR mode Be aware that code line shown in Figure 9 may change with updates done in clocks using Config Tools. Note 2. Configure DCDC in continuous mode. According to KW36 Reference Manual, the use of BLPE in VLPR mode is only feasible when the DCDC is configured for continuous mode. First, let's define gDCDC_Enabled_d flag to 1 on preprocesor. With this implementation, the use of DCDC_Init function will be enabled, and it's where we going to add the code line to enable continuous mode. Right click on your project, select Properties, go to Settings under C/C++ Build, then Preprocessor under MCU C Compiler (Figure 10).   Figure 10. MCUXpresso Preprocessor   Click on add button from Defined symbols, write gDCDC_Enabled_d=1 and click OK to finish (Figure 11).  Re-compile your project. Figure 11. MCUXpresso Defined symbols   Now let's set VLPR_VLPW_CONFIG_DCDC_HP bits to 1 from DCDC_REG0 register. Figure 12 was taken from KW36 Reference Manual. Figure 12. VLPR_VLPW_CONFIG_DCDC_HP values. Go to DCDC_Init  function and add the next code line to enable continuous mode on DCDC: DCDC->REG0 |= DCDC_REG0_VLPR_VLPW_CONFIG_DCDC_HP_MASK; Figure 13 shows the previous code line implemented in firmware project inside of DCDC_Init function. Figure 13. Continuous mode for DCDC enabled. 3. Configure MCU into VLPR mode To finish, let's write the code to configure MCU into VLPR power mode. Copy and paste next code just after doing implementation described on step 1 and 2: #if (defined(FSL_FEATURE_SMC_HAS_LPWUI) && FSL_FEATURE_SMC_HAS_LPWUI) SMC_SetPowerModeVlpr(SMC, false); #else SMC_SetPowerModeVlpr(SMC); #endif while (kSMC_PowerStateVlpr != SMC_GetPowerModeState(SMC)) { } It may be needed to add the SMC library: #include "fsl_smc.h" The code is configuring MCU into VLPR mode with bits RUNM from SMC_PMCTRL register (Figure 14) and then check if it was correctly configured by reading status bits PMSTAT from SMC_PMSTAT register (Figure 15) Figure 14. RUNM bits from SMC_PMCTRL register. Figure 15. PMSTAT bits from  SMC_PMSTAT register. KW36 is ready to operate and BLPE or BLPI clocking modes with VLPR power mode.
查看全文
FRDM-KW36 Software Development Kit (SDK) includes drivers and examples of FlexCAN module for KW36 which can be easily configured for a custom communication. For example, if user want to change the default baud rate from FlexCAN driver demo examples then the only needed change is the default value on "config->baudRate" and "config->baudRateFD" from "FLEXCAN_GetDefaultConfig" function (See Figure 1). Segments within a bit time will be automatically configured to obtain the desired baud rate. By default, demos are configured to work with CAN FD communication. Figure 1. FRDM-KW36's default baudrate from flexcan_interrupt_transfer driver example Even so, there are cases where segments within a bit time are not well configured and it's necessary that user configure segments manually. An example occurs by setting the maximum FD baud rate "3.2MHz" using the 32MHz xtal or "2.6MHz" using a 26MHz xtal where demo reports an error. See Figure 2. Figure 2. Error by setting maximum baud rate When this error occurs, the fix is on setting the timing config parameters correctly by including the definition of SET_CAN_QUANTUM on application source file (see Figure 3) and then declare and initialize the timing config parameters shown in Figure 4. Figure 3. SET_CAN_QUANTUM define Figure 4. Custom timing config parameters For this example we are going to show how to calculate timing config parameters in an scenario where a CAN FD communication is used with baud rate of 500kHz on nominal phase and 3.2MHz on FD phase. See Figure 5.  To do it, we need to calculate Time Quanta and value of segments within the bit time.    Figure 5. Custom CAN FD baudrate KW36 Reference Manual in chapter "37.4.8.7 Protocol timing" shows the segments within a bit time for CAN nominal phase configured in "CAN_CTRL1" register (see Figure 6), and segments for FD phase configured in CAN_FDCBT register (see Figure 7). Figure 6. Segment within a bit time for CAN nominal phase Figure 7. Segment within a bit time for CAN FD phase Before calculating the value of segments, first we need to calculate the Time Quanta which is the atomic number of time handled by the CAN engine. The formula to calculate Time Quanta is shown in Figure 8 taken from KW36 Reference Manual. Figure 8. Time Quanta Formula CANCLK can be selected by CLKSRC bits on CAN_CTRL1 register as shown in Figure 9, where the options are Peripheral clock=20MHz or Oscillator clock (16MHz if using 32MHz xtal or 13MHz if using 26MHz xtal). The recomiendation is to use the Oscillator clock due to peripheral clock can have jitter that affect communication.  Figure 9. CAN clocks To select the Oscillator clock, search for flexcanConfig.clkSrc definition and set it to kFLEXCAN_ClkSrcOsc as shown in Figure 10. Figure 10. CANCLK selection Next step is selecting the PRESDIV value for nominal phase and FPRESDIV for FD phase. You have to select the right value to achieve the TQ needed to obtain the configured baudrate. For this example, let's set FPRESDIV value to 0 and PRESDIV value to 3. TQ calculation for nominal phase: TQ = (PRESDIV + 1) / CANCLK = (3 + 1) / 16000000 = 0.00000025 TQ calculation for FD phase: TQ = (FPRESDIV + 1) / CANCLK = (0 + 1) / 16000000 = 0.0000000625 The bit rate, which defines the rate of CAN message is given by formula shown in Figure 11 taken from KW36 Reference Manual. Figure 11. CAN Bit Time and Bit Rate Formulas With this info and with our TQ calculated, we can deduce that we need: For Nominal phase: 8 = Number of Time Quanta in 1 bit time For FD phase: 5 = Number of Time Quanta in 1 bit time Now, let's define the value of segments. For nominal phase: Bit Time =  (number of Tq in 1 bit time) x Tq CAN Bit Time = (1 + (PROPSEG + PSEG1 + 2) + (PSEG2 + 1) ) x Tq CAN Bit Time = (1 + (1 + 2  + 2) + (1 + 1) ) x Tq = 8 x 0.00000025 =  Baud rate = 1/ CAN Bit Time = 500KHz For FD phase: CAN Bit Time = (number of Tq in 1 bit time) x Tq CAN Bit Time = (1 + (FPROPSEG + FPSEG1 + 1) + (FPSEG2 + 1) ) x Tq CAN Bit Time = (1 + (0 + 1 + 1) + (1 + 1) ) x Tq = 5 x Tq =  0.0000003125 Bit Rate = 1/CAN Bit Time = 1 / 0.0000003125 =  3.2MHz To finish, just update the calculated values on your firmware on flexcanConfig.timingConfig structure.  Notes: FRDM-KW36 Software Development Kit (SDK) can be downloaded from MCUXpresso webpage. FlexCAN driver examples are located in path: "SDK_2.2.0_FRDM-KW36\boards\frdmkw36\driver_examples" from your downloaded FRDM-KW36 SDK. Take in consideration that not all the baud rates are achievables and will depend on the flexcan clock and segment values used.
查看全文
By default, FRDM-KW36 board includes a 32MHz XTAL (YI) as shown in Figure 1 but there are cases where a 26MHz XTAL is needed instead of 32MHz XTAL for FRDM-KW36 or a custom KW36 board.   Figure 1. 32MHz XTAL from FRDM-KW36 schematics Wireless connectivity demos from FRDM-KW36 Sofware Development Kit are configured to run with a 32MHz XTAL by default, but it's very easy to modify the software to operate with a 26MHz XTAL. Follow next steps to configure a FRDM-KW36 wireless connectivity demo to operate with a 26MHz XTAL: 1. In clock_config.h file, change BOARD_XTAL0_CLK_HZ define from 32000000U to 26000000U as shown in Figure 2.   Figure 2. BOARD_XTAL0_CLK_HZ define in clock_config.h 2. Add RF_OSC_26MHZ=1 line in preprocessor: If using IAR IDE: Right click on your project, then click options (Figure 3). Figure 3. IAR project options Go to C/C++ Compiler tab, then Preprocessor, and add RF_OSC_26MHZ=1 line in defined symbols window (Figure 4). Figure 4. IAR Preprocessor If using MCUXpresso IDE: Right click on your project, select Properties, go to Settings under C/C++ Build, then Preprocessor under MCU C Compiler (Figure 5). Figure 5. MCUXpresso Preprocessor Click on add button from Defined symbols, write RF_OSC_26MHZ=1 and click OK to finish (Figure 6). Figure 6. MCUXpresso Defined symbols To finish, re-compile your project and it will be ready to operate with a 26MHz XTAL. FRDM-KW36 SDK can be downloaded from the MCUXpresso webpage.
查看全文
All FSCI packets contain a checksum field to verify data integrity. Every time a FSCI packet is created (by the Host or a Kinetis device) a new CRC is calculated based on every data byte in the FSCI frame. Compute CRC for TX packet The CRC field is calculated by XORing each byte contained in the FSCI command (opcode group, opcode, payload length and payload data). Checksum field then, accumulates the result of every XOR instruction.    In the firmware, the CRC is calculated in the 'FSCI_transmitPayload()' function wich is located in '<HSDK project>/framework/FSCI/Source/FsciCommunication.c' file. See FSCI_computeChecksum(). Example: TX: AspSetXtalTrim.Request 02 95 0A 01 30 AE    Sync            [1 byte] = 02    OpGroup     [1 byte] = 95    OpCode      [1 byte] = 0A    Length         [1 byte] = 01    trimValue     [1 byte] = 30    CRC            [1 byte] = AE     <------- (0x95) XOR (0A) XOR (0x01) XOR (0x30) = 0xAE Disable CRC field validation Every time a FSCI packet is received, the device verifies the checksum value.  The next changes will allow the board to receive FSCI packets without verifying the CRC field. However, the board will send the FSCI responses to the Host with this CRC field. Go to 'FsciCommunication.c' file. Search for 'fsci_packetStatus_t FSCI_checkPacket( clientPacket_t *pData, uint16_t bytes, uint8_t* pVIntf )' function. Comment all line codes related to checksum verifying. The image below shows what has to be commented. Compile project and load it to the board. Verify functionality with Test Tool. Select any command and check Raw Data checkbox. Delete the CRC data field and send the FSCI message pressing Send Raw. The loaded command set will vary depending on the demo you are using (Thread, ZigBee, BLE, etc.). The FSCI message is sent without a CRC field and the board responses to the command successfully.
查看全文
General summary MCUBOOT, fsci_bootloader and otap_bootloader are 3 different bootloader applications that can be used depending on the use case. The MCU Flashloader is a separate implementation but it's also mentioned to avoid misunderstanding.   MCUBOOT The MCU bootloader provides support for multiple communication protocols (UART, SPI, I2C, CAN) and multiple applications to interface with it. Summary: - It's a configurable flash programming utility that operates over a serial connection on several Kinetis MCUs. - Host-side command line (blhost) and GUI tools are available to communicate with the bootloader.  -  By default, application starts at address 0xa000. - MCU Bootloader|NXP website - MCU Bootloader Reference Manual - MCU Bootloader Demo Application User's Guide   fsci_bootloader Framework Serial Connectivity Interface (FSCI) is an NXP propietary protocol that allows interfacing the Kinetis protocol stack with a host system or PC tool using a serial communication interface. The FSCI bootloader enables the FSCI module to communicate with the PC and transfer the image using the FSCI protocol. Summary: - It relies on the FSCI protocol to transfer the binary from a PC connected via UART, using a python and C applications. - To enter into bootloader mode (in FRDM-KW41Z), hold SW1 (Reset) and press SW4, then release SW1 first and SW4 second. Please refer to demo user's guide to get the specific steps for your platform. - By default, application starts at 0x4000. - FSCI Bootloader Manual   otap_bootloader The Connectivity SDK contains Over-the-Air firmware upgrade examples. The OTAP bootloader loads an image obtained from wireless communication, the OTAP bootloader only enters after an image was successfully transferred to the client device (internal or external flash). Summary: - It's used by over the air programmed devices. - The bootloader mode only enters if a flag is set after reset triggered by a successful reception of an image over the air. - By default, application starts at 0x4000. - Kinetis Thread Stack Over-the-Air (OTA) Firmware Update User’s Guide   mcu_flashloader The MCU flashloader is a specific implementation of the MCU bootloader. For the flashloader implementation, the MCU bootloader command interface is packaged as an executable that is loaded from flash and executed from RAM. This configuration allows the user application to be placed at the beginning of the on-chip flash where it is automatically launched upon boot from flash. Using the MCU flashloader to program a user application to the beginning of the flash makes this implementation of the bootloader a one-time programming aid. The MCU flashloader doesn't allow to jump to a different section after a timeout or button press like the other bootloaders, it's main purpose is to flash an application without the need of an external debugger, mainly used for factory programming. Summary: - It is pre-programmed into many Kinetis flash devices during manufacturing and enables flash programming without the need for a debugger. - After the user application is programmed into flash memory, the Kinetis flashloader is no longer available. - Documentation: Getting Started with the MCU Flashloader   You can select from the MCU Bootloader, FSCI_Bootloader and OTAP Bootloader, depending on your needs. JC
查看全文
QTool is a PC software tool that works with QN9080 USB dongle to assist in the development of BLE projects with the QN9080. You control the dongle via the QTool software, which issues and receives FSCI (Framework Serial Communication Interface) formatted commands over a virtual COM port. The dongle can then act either as a master or a slave to a QN9080DK board over BLE.  Before using the BLE dongle with QTool though, the firmware on the QN9080 Dongle must be updated. The updated firmware can be found inside the QTool installation directory, and you will need to put the dongle into bootloader mode to drag-and-drop new firmware on it. Updating the Firmware on the QN9080 Dongle. 1. Install QTool: https://www.nxp.com/webapp/sps/download/license.jsp?colCode=Connectivity-QTool-Setup   2. Plug the QN9080 Dongle into a USB port on your computer 3. Using a wire, connect TP5 to ground. You can use either TP4 or the USB shield for GND. 4. While that wire is connected, press the reset button on the dongle. This will now put the dongle into bootloader mode. 5. A drive will enumerate on your computer named “CRP_DISABLD”     6. You can now remove the wire 7. Delete the firmware.bin file found in that drive 8. Drag-and-drop the firmware.bin file found in C:\NXP\Connectivity QTool\bin files into that enumerated drive. 9. Once done copying, unplug and replug in the USB Dongle, and the new firmware will now be running.  Installing the QN9080 Dongle Driver The dongle will enumerate as a USB CDC COM device. If the CDC driver is not automatically detected, you will need to manually install the driver. 1. Right-click Computer and choose Properties, the System Management window appears. 2. Click Device Manager and navigate to MCU VIRTUAL COM DEMO      3. Right-click the device MCU VIRTUAL COM DEMO and choose Update Driver Software 4. Click the  Browse my computer for driver software option in the window. 5. Click Browse button to go to the folder  C:\NXP\Connectivity QTool\drivers 6. Click the Next button at the bottom to install the driver.  7. After the driver is installed you will see the Virtual Com Port device under the Ports category    Using QTool: Now that the QN9080 dongle has the updated firmware and has the correct driver installed, you can follow the instructions in the QTool documentation found at C:\NXP\Connectivity QTool\UM11085.pdf Related documentation: QN908x Quick Start Guide QN908x DK User's Guide
查看全文
This Document describes the additional changes needed for JN-AN-1229 ZigBee PRO Application Template for ZigBee version 1002 to be able to compile correctly with the latest update SDK JN-SW-4170 Version 1745 and JN-SW-4270 Version 1746. Note:  These modifications can be also found in the JN516x ZigBee 3.0 SDK Release Notes v1745 (Chapter 4.3 Modifications Required) Tool modifications The .zpscfg file contains all the information available of the setup of the ZigBee network, this file it’s located in C:\...\...\workspace\ JN-AN-1229\Common The first step is to add the MAC Interface List to The ZigBee devices (Co-ordinator, Router, and Sleeping End Device) in the .zpscfg file. Then, add the MAC Interface selecting the New Child option. In the Properties tab, the Co-ordinator and the Router should have the Router Allowed option set to True. Stack modifications The new stack has support for better throughput and automatic buffering of data packets during route discovery. This requires the addition of a new queue in the application. Open the app_common.h file which it’s located in the Common folder. This queue should be tied to the stack definition: extern PUBLIC tszQueue zps_msgMcpsDcfm; After that, open the app_router.c and app_sleeping_enddevice.c. The ZPS_tsAplAib structure has been changed, so, the vStartup function should be modified Old version /* Set channel to scan and start stack */ ZPS_psAplAibGetAib()->apsChannelMask = 1 << u8Channel; Update needed /* Set channel to scan and start stack */ ZPS_psAplAibGetAib()->pau32ApsChannelMask[0] = 1 << u8Channel; Add the next code to the app_start.c(Coordinator and Router) and app_start_SED.c(Sleeping End Device) The buffer of the Router device should be modified. The size of the queue is defined as: #define MCPS_DCFM_QUEUE_SIZE 5 The storage of the queue must be defined: PRIVATE MAC_tsMcpsVsCfmData asMacMcpsDcfm[MCPS_DCFM_QUEUE_SIZE]; In the APP_vInitResources function an additional queue must be added: ZQ_vQueueCreate(&zps_msgMcpsDcfm, MCPS_DCFM_QUEUE_SIZE,  sizeof(MAC_tsMcpsVsCfmData),(uint8*)asMacMcpsDcfm);  
查看全文
The “BeyondStudio for NXP” Integrated Development Environment (IDE) provides a platform for the development of wireless network applications to be run on NXP’s JN516x family of wireless microcontrollers. For more details and installation guide.  JN-UG-3098 (BeyondStudio for NXP Installation and User Guide). This document explains the common issues that the user will face when trying to develop a new application using BeyondStudio IDE.   First of all, be sure that you are working with the latest SDK version and application note.    Import Problems After you import some application note that you want to take as reference. 2.2 Importing a Project. BeyondStudio for NXP Installation and User Guide.     1. Wrong Path A  common issue is a user uses another path for the installation of the SDK than the default one (C:\nxp\bstudio_nxp\workspace). When trying to find the Makefile ("SDK/JN-SW-4168/Stack/Common/Build/config.mk"), the IDE uses a relative path, for that reason it assumes that the file is in the correct directory. As the path was changed, the file can’t be found.   2.Project Directory After you select the Application Note (AN) you want to import remember that there will be an option for the JN517x as most of the projects are compatible between them (Zigbee 3.0, ZigBee Link Light). Nonetheless, BeyondStudio is not compatible with the JN517x.  While importing the project you only must select the JN516x project and none of the options must not be selected.     Linking Errors Open a source file (.c) or a header file (.h),  you will notice that the IDE shows a lot of errors even though the project has not been compiled yet. The errors you are seeing is Eclipse not being able to resolve various variables and functions within the SDK. You might see some errors like: Symbol “xxx” could not be resolved for example. After starting the compilation process, look at the console log and notice that the bin file is being generated correctly. Do not try to add another file in the path and Symbols trying to avoid all those errors; the IDE will look for the includes that the project needs. If you used the default path location, it will not have any problem with the compilation. The OS_Gen, ZPS_Gen, and PDUM_Gen, for example, are all files automatically generated based on the configuration files, performing a clean will remove those files but will be created again after a new compilation. File app.zpscfg Problems Encountered The next error will appear if the Zigbee Plug-in is not installed. Follow the installation procedure for the plug-ins 1.2.3 Installing the ZigBee Plug-ins BeyondStudio for NXP Installation and User Guide. Look at the installation folder that is included in the SDK. C:\NXP\bstudio_nxp\sdk\JN-SW-41xx\Tools\Eclipse_plugins\com.nxp.sdk.update_site For a better reference the ZPS Configuration Editor provides a convenient way to set ZigBee network parameters ZigBee PRO Stack User Guide I hope it helps. Regards, Mario
查看全文
Hello all, let me share a video demonstration of the Thread Smart Home model. See the link below: Thread Smart Home model Best regards, Karel
查看全文
This document describes how to add additional cluster to the Router application in the JN-AN-1217 ZigBee 3.0 Base Device Application Note. The Router application's main endpoint contains Basic, Groups, Identify and OnOff server. The steps below describe how to add two clusters to Router: Temperature Measurement server and OnOff client. Note that these changes only go as far as making the new clusters added and discoverable, no functionality has been added to these clusters.  Common/Source/app.zpscfg The first step is to update the ZigBee PRO Stack Configuration file to add the new clusters (OnOff Client, Temperature Measurement Server) to the Router application endpoint. The HA profile already contains few clusters but Temperature Measurement cluster was added:   The OnOff client was already present in Router endpoint but the Temperature Measurement cluster was then added into Router application endpoint:   Router/Build/Makefile For cluster belonging to General domain, the cluster code is automatically build and linked but for other domains, the compiling and linking needs to be enabled. As Temperature Measurement belongs to Measurement and Sensing domain, enable the cluster code in Makefile: Router/Source/zcl_options.h This file is used to set the options used by the ZCL. Enable Clusters The cluster functionality for the router endpoint was enabled:   Enable any optional Attributes and Commands for the clusters  Add the cluster creation and initialization into ZigBee Base device definitions The cluster functionality for some of the clusters is already present on ZigBee Base Device. For Temperature Measurement cluster the functionality was added into ZigBee Base Device. <Path to JN-SW-4x70 SDK>/ Components/ZCL/Devices/ZHA/Generic/Include/base_device.h The first step was including the Temperature Measurement header files into base device header file as shown below:   The second step was adding cluster instance into base device Instance as shown below: The next step was to define the cluster into the base device structure as below: <Path to JN-SW-4x70 SDK>/ Components/ZCL/Devices/ZHA/Generic/Include/base_device.c The cluster create function for Temperature Measurement cluster for server was called in ZigBee base device registration function:   Router/Source/app_zcl_task.c Temperature Measurement Server Cluster Data Initialization - APP_vZCL_DeviceSpecific_Init() The default attribute values for the Temperature Measurement clusters are initialized:
查看全文
802.15.4 wireless sniffers like the USB-KW41Z are capable of capturing over-the-air traffic. The captured packets are passed to a network protocol decoder like Wireshark over a network interface tunnel built by the Kinetis Protocol Analyzer.   Hardware  One USB-KW41Z preloaded with sniffer firmware ( instructions found at www.nxp.com/usb-kw41z )  Software Download & Install Thread Wireshark from wireshark.org which is an open-source network protocol analyzer capable of debugging over the air communication between Thread devices. Kinetis Protocol Analyzer is a software that provides a bridge between the USB-KW41 and Wireshark.  Wireshark Configuration  Open Wireshark from the Program Files Click Edit and select Preferences  Click Protocols to expand a list of protocols Select IEEE 802.15.4, click the Decryption Keys Edit... button Create a new key entry by pressing the plus button, then set the following values and click OK       Decryption key = 00112233445566778899aabbccddeeff      Decryption key index = 1      Key hash = Thread hash Find CoAP and configure it with CoAP UDP port number = 5683 Click Thread and select Decode CoAP for Thread  with Thread sequence counter = 00000000 as shown below At the 6LoWPAN preferences, add the Context 0 value of fd00:0db8::/64 Click OK and close Wireshark Configure Kinetis Protocol Analyzer  Connect the USB-KW41Z to one of the USB ports on your computer Open the device manager and look for the device connected port Open the "Kinetis Protocol Analyzer Adapter" program Make sure, you have a USB-KW41Z connected to your PC when opening the program because the Kinetis Protocol Adapter will start looking for kinetis sniffer hardware. Once the USB-KW41Z is detected, the previously identify COM port will be displayed Select the desired IEEE 802.15.4 channel to scan in the Kinetis Protocol Analyzer window. This guide selects channel 12 as an example  Click on the Wireshark icon to open Wireshark Network Protocol Analyzer An error may appear while opening Wireshark, click OK and continue Wireshark Sniffing Wireshark Network Analyzer will be opened. On the "Capture" option of the main window, select the Local Area Connection that was created by the Kinetis Protocol Analyzer, in this example, Kinetis Protocol Analyzer created "Local Area Connection 2", then click "Start" button. USB-KW41Z will start to sniff and upcoming data will be displayed in the "Capture" window of the Wireshark Network Protocol Analyzer.
查看全文
High level description to enable a Linux + KW41Z Border Router. Similar to how it’s shown for the K64 solution in the Kinetis Thread Stack Application Development Guide.   Configure the OpenWrt router to assign the IPv6 ULA prefix 2001:2002:2003::/48. On the LAN network, the router distributes addresses from range 2001:2002:2003::/60 Plug an Ethernet cable between the OpenWrt router and the Linux box. Before creating the Thread network, the Linux box has a global address on its eth interface from range 2001:2002:2003::/60. After creating the Thread network, the BR configures on its Serial TAP interface an address from range 2001:2002:2003::/60. On its 6LoWPAN interface, the BR configures an address from range 2001:2002:2003:c::/64. This is achieved with DHCPv6 prefix delegation - the router is requested to assign a new prefix space to be used by the Thread network. The forth segment in the IPv6 range might be 2, 4, 8 or c, depending of the number of DHCP-PD requests made to the router. After 4 attempts, the router will not lease any other prefixes for some time. In order to force that, you'd require to restart the odhcpd deamon in the OpenWrt router with the following command: /etc/init.d/odhcpd restart . Join the router eligible device, which configures an address in 2001:2002:2003::1/60. We then ping the "Internet" (the LAN interface on the OpenWrt router) and it works. “threadtap0” interface must be bridged with an uplink interface connected to an OpenWrt DHCPv6-PD enabled router; it will act identically as the K64F solution.   Setup Linux PC (Ubuntu) OpenWrt AP/Router with DHCPv6-PD support (OpenWrt version used in this guide: OpenWrt Chaos Calmer 15.05.1) For reference, hardware used on this guide: TP-Link Model TL-WR741ND 150Mbps Wireless N Router OpenWRT firmware supports multiple hardware available at https://openwrt.org/ 1 FRDM-KW41Z (Host Controlled Device, connected to Linux) 1 FRDM-KW41Z (Router Eligible Device or any joiner device) Thread version 1.1.1.20 (from SDK builder at mcuxpresso.nxp.com)   Host Controlled Device firmware, make sure the following macros are enabled: THR_SERIAL_TUN_ROUTER                       /source/config.h     -> Enables TAP interface by default (not TUN) THR_SERIAL_TUN_ENABLE_ND_HOST     /app/common/app_serial_tun.h   OpenWRT router Configure IPv6 ULA-Prefix:   Linux Copy HSDK folder Create 'threadtap0' TAP interface: …/host_sdk/hsdk/demo#   sudo bash make_tap.sh Use "Thread_Shell" or modify “Thread_KW_Tun” demo to enable the SERIAL_TAP macro …/host_sdk/hsdk/demo#   nano Thread_KW_Tun.c #define SERIAL_TAP 0   modify to:  #define SERIAL_TAP  1        Note: For demo purposes, the "Thread_Shell" demo is recommended, it already uses TAP by default and allows input commands. If this is not required and only the TAP bridge is to be used, use the Thread_KW_Tun demo. Bridge the interfaces; assuming eno1 is the interface connected directly to OpenWrt: # brctl addbr br0 # brctl addif br0 eno1 # brctl addif br0 threadtap0 # ifconfig br0 up Note: (Optional) Addresses on the bridged interfaces are lost and need to be reconfigured on the actual bridge. In this example, after bridging eno1 (interface to OpenWrt router), you’d have to run #dhclient br0 to get an IPv4 address on br0 for SSH to the router and/or #dhclient -6 br0 to get an IPv6 address to the br0 interface. There's a note here https://wiki.archlinux.org/index.php/Network_bridge#With_bridge-utils  about this.   Build C demos …/host_sdk/hsdk/demo#   make Run Thread_Shell or Thread_KW_Tun demo. …/host_sdk/hsdk/demo#   sudo ./bin/Thread_Shell /dev/ttyACM0 threadtap0 25 or …/host_sdk/hsdk/demo#   sudo ./bin/Thread_KW_Tun /dev/ttyACM0 threadtap0         Note: Try to run the demo without parameters to get some help on the input parameters   ifconfig Thread_Shell demo Thread_KW_Tun demo Joiner FRDM-KW41Z (shell) Join the Thread network Verify IP addresses Ping Eth LAN interface on OpenWrt router to verify “Internet” connectivity  Regards, JC
查看全文
The attached PDF file contains two A3 format "posters". The first one summarize the contents of the SMP Pairing Request and SMP Pairing Response packets (BLE 4.2). It shows how are the sub-fields of these packets set and what do they represent. The second one contains a diagram which summarizes how the pairing method and it's properties are determined during the SMP Pairing procedure for both BLE Legacy Pairing (BLE4.0 and BLE 4.1) and BLE Secure Connections Pairing with ECDH (BLE 4.2). Some of the tables in the diagram are taken from the BLE Specification. If you find any errors or have any suggestions of improvement please leave a comment or send me a message. Preview:
查看全文