Max input voltage of PSWITCH and DCDC_CFG pins on MKW40

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Max input voltage of PSWITCH and DCDC_CFG pins on MKW40

Max input voltage of PSWITCH and DCDC_CFG pins on MKW40

Our customer, who is considering MKW40, is asking NXP regarding max input voltage of PSWITCH and DCDC_CFG pins.

Especially they plan to use buck mode with input voltage 4.2[v] as shown below.

Would you comment if max voltage of PSWITCH and DCDC_CFG pins is 4.2[v] as well as DCDC_IN pin?

pastedImage_0.png

Regards,

Koichi

ラベル(1)
コメント

Hi Koichi,

The above configuration shall work without any problem. According to chip reference manual, chapter DCDC, in buck configuration mode, DCDC_IN voltage is between 1.8V and 4.2V, the DCDC_CFG is tied to DCDC_IN and PSWITCH will also be tied to DCDC_IN each time the pushbutton is pressed. Please see the below picture from reference manual.

pastedImage_0.png

Regards,

Mihai

Hello Andrei,

Thank you for your comment.

According to your comment, do you plan to update MKW40 datasheet?

Because our customer want NXP's guarantee with MKW40 datasheet.

Regards,

Koichi

評価なし
バージョン履歴
最終更新日:
‎01-11-2016 11:14 PM
更新者: