KW37_38_39 DCDC converter.pdf

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW37_38_39 DCDC converter.pdf

KW37_38_39 DCDC converter.pdf

This application note describes the usage of the DC-DC Switching Mode Power Supply (SMPS) converter for the MKW39A/38A/37A/38Z/37Z families. This document covers operating voltages, types of circuit operation, hardware design guidelines, software configuration, and power capabilities.

It's a complementary document from the AN5025.

The DC-DC converter for MKW3x is a dual output converter that supports two operating modes: Bypass and Buck. In Bypass mode, the DC-DC converter is disabled and the supply pins of the microcontroller must be supplied externally. In Buck mode, the DC-DC converter is enabled and requires a DC supply in the range of 1.8 V to 4.2 V (during startup the minimum required is 2.1 V).

Labels (1)
Attachments
No ratings
Version history
Last update:
‎05-11-2020 06:07 AM
Updated by: