KW37_38_39_Bluetooth LE Range Performance.pdf

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW37_38_39_Bluetooth LE Range Performance.pdf

KW37_38_39_Bluetooth LE Range Performance.pdf

This document provides information on distance measurements depending of the Bluetooth LE data rate (1Mbps, 2Mbps, LR S=2 & LR S=8).

The FRDM-KW38 boards are used to perform the measurements.

Results are similar on KW37 and KW39.

 

Labels (1)
Attachments
Comments
100% helpful (2/2)
Version history
Last update:
‎05-11-2020 05:48 AM
Updated by: