Enabling i.MX8MP-EVK uSDHC1 M.2 For WiFi on Android-11.0.0_2.6.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Enabling i.MX8MP-EVK uSDHC1 M.2 For WiFi on Android-11.0.0_2.6.0

Enabling i.MX8MP-EVK uSDHC1 M.2 For WiFi on Android-11.0.0_2.6.0

Some users want to use SDIO signals on M.2 connector for WiFi card. In default linux bsp, there is no problem using imx8mp-evk-usdhc1-m2.dts, usdch1 driver can normally loaded, and detect WiFi module, But default android bsp doesn't support it, even if using corresponding device tree, usdch1 driver can NOT be loaded correctly, Because default android bsp doesn't load pwrseq_simple.ko, which is used by usdhc1 node. Detailed steps on enabling usdhc1 in the attached document, hope it can help users who wants to use M.2 SDIO WiFi card.

[Note]

For other android bsp version, users can also refer to the steps in attached document.

 

Thanks!

Regards,

Weidong Sun

附件
无评分
版本历史
最后更新:
‎07-31-2024 07:13 PM
更新人: