wlan 88W9098

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

wlan 88W9098

872 Views
Mike17
Contributor I

It's very easy and random for me to meet crash 

the crash dump as the following

driver information Driver version = PCIE9098--17.68.1.p81-MXM5X17277-GPL-(FP68) 

Is there anyone know how to fix it?

Exception Class: Kernel (KE)
PC is at [<ffffff8000f37210>] wlan_process_bypass_tx+0x88/0x254 [mlan]
LR is at [<ffffff8000f371fc>] wlan_process_bypass_tx+0x74/0x254 [mlan]

Current Executing Process:
[kworker/u9:1, 1317][kthreadd, 2]

Backtrace:
[<ffffff80080d7544>] notifier_call_chain+0x6c/0x90
[<ffffff80080d75fc>] atomic_notifier_call_chain+0x38/0x4c
[<ffffff80080d7d00>] notify_die+0x24/0x30
[<ffffff800808f8c0>] die+0xc4/0x1e8
[<ffffff8008b24a40>] die_kernel_fault+0x64/0x78
[<ffffff80080a4834>] __do_kernel_fault+0xd4/0x100
[<ffffff80080a4d50>] do_translation_fault+0x90/0x98
[<ffffff8008080d78>] do_mem_abort+0x68/0x100
[<ffffff8008082bc0>] el1_da+0x18/0xac
[<ffffff8000f37210>] wlan_process_bypass_tx+0x88/0x254 [mlan]
[<ffffff8000f3442c>] mlan_main_process+0x5cc/0x894 [mlan]
[<ffffff80011f40e0>] woal_main_work_queue+0x7c/0x9d0 [moal]
[<ffffff80080ce0e0>] process_one_work+0x204/0x34c
[<ffffff80080cf1e0>] worker_thread+0x264/0x350
[<ffffff80080d4538>] kthread+0x120/0x134
[<ffffff80080859a0>] ret_from_fork+0xc/0x18
[<fffffffffffffffb>] 0xfffffffffffffffb

0 Kudos
Reply
1 Reply

861 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @Mike17 

Tell me information below, please!

1. which platform?

2. which linux kernel version?

3. if possible, can you send me schematic ?

 

Thanks!

Regards,

weidong

 

0 Kudos
Reply