wlan 8897 Wakeup card timeout issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

wlan 8897 Wakeup card timeout issue

7,549 Views
PeterYang_TW
Contributor I

Hello NXP Team,

We use Synaptics chip as a host and our Wi-Fi chip is 8897.
If our system entered standby, we found Wi-Fi and BT can't work after some hours.

We got the following errors:
[40901.633724] Wakeup device...
[40902.573041] CPU3: update max cpu_capacity 853
[40902.670385] logd: logdr: UID=1000 GID=1000 PID=1216 n tail=0 logMask=4 pid=0 start=0ns timeout=0ns
[40903.762661] wlan0:
[40903.762669] QUEUE_CMD: cmd=0xd1 is queued
[40904.701838] logd: logdr: UID=1000 GID=1000 PID=1216 n tail=0 logMask=4 pid=0 start=0ns timeout=0ns
[40904.713041] wlan_wakeup_card_timeout_func: ps_state=3
[40904.713046] Wakeup card timeout!
[40904.713052] event id:0x80000012
[40904.713061] Driver version = SD8897-15.68.19.p59-C3X15C698-GPL-(FP68)
[40904.713063] main_state = 4
[40904.713065] ioctl_pending = 1
[40904.713067] tx_pending = 4

We can reproduce this issue on SD8897-15.68.19.p59.1-C3X15CS698.p1-GPL-(FP68) and SD8897-15.68.19.p18-C3X15C612-GPL-(FP68).

Please help us provide a patch to fix this issue.

Attached is the log file and this message(wlan_wakeup_card_timeout_func) is at line 80523. 

BR,
Peter 

Labels (2)
0 Kudos
Reply
14 Replies

7,503 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi @PeterYang_TW ,

 

Try the command of loading driver:

insmod sd8897.ko driver host_mlme=1 drvdbg=0x6 cfg80211_wext=0xf sta_name=wlan wfd_name=p2p max_vir_bss=1 ps_mode=1 auto_ds=1 drv_mode=7 p2p_enh=1 wakelock_timeout=30  cal_data_cfg=cal_data.conf 

 

Regards,

weidong

0 Kudos
Reply

7,498 Views
PeterYang_TW
Contributor I

Hi @weidong_sun,

What are ps_mode=1 and auto_ds=1?
Could you list all the values and its meaning for ps_mode and auto_ds?

We will try this command that you provided.

Thanks.
Peter

0 Kudos
Reply

7,484 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @PeterYang_TW ,

 

ps_mode=1, 802.11 power saving mode is supported.

ps_mode=2, 802.11 power saving mode is disabled.

auto_ds=1, chip will automatically enter deep sleep mode.

audo_ds=2, automaical deep sleep function is disable.

 

So 

ps_mode=1 & auto_ds=1 means the chip supports power saving mode.

ps_mode=2 & auto_ds=2 means the chip will not enter into power saving mode.

 

Regards,

weidong

 

0 Kudos
Reply

7,479 Views
PeterYang_TW
Contributor I

Hi @weidong_sun,

Thank you for the information.

I have another question.
If we didn't set ps_mode and auto_ds, what's the default setting after loading driver?
We want to find the root cause of this issue.

BR,
Peter

0 Kudos
Reply

7,463 Views
PeterYang_TW
Contributor I

Hi @weidong_sun,

This issue can be reproduced with ps_mode=1 auto_ds=1.
Attached is the test log. Could you help us analyze the log to find the root cause?

BR,
Peter

0 Kudos
Reply

7,453 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @PeterYang_TW ,

 

Please set ps_mode=2 auto_ds=2 !

Then try it. and tell me result, please!

 

Regards,

weidong

0 Kudos
Reply

7,449 Views
PeterYang_TW
Contributor I

Hi @weidong_sun,

We tested with ps_mode=2 auto_ds=2 and WiFi still works fine after 50 hours.

I referred to this discussion https://community.nxp.com/t5/Wireless-Connectivity/SD9098-quot-abnormal-driver-state-quot/m-p/149581... to set ps_mode=2 and auto_ds=2 when loading driver. 

We still want to know the root cause.

Thanks,
Peter

0 Kudos
Reply

7,441 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @PeterYang_TW ,

 

When setting ps_mode=1 & auto_ds=1 , chip will automatically enter into power savming mode, and AP's beacon frame will wake it up.

If your host does not have a hardware wake-up mechanism to connect to WIFI, when your host wakes up, the wifi is still in sleep.
For example:
If there is a GPIO on the host side connected to WIFI (wake-up pin), when the host wakes up, it will also wake up the wifi.

 

Regards,

weidong

0 Kudos
Reply

7,432 Views
PeterYang_TW
Contributor I

Hi @weidong_sun,

Thank you for your information.

These two pictures are our wifi electrical diagram. Our host has a hardware wake-up mechanism to connect to WIFI. When the "Wakeup card timeout" occurred, our host was still on standby.
The root cause doesn't look like "when your host wakes up, the wifi is still in sleep."

PeterYang_TW_0-1679016781115.png

PeterYang_TW_2-1679017119316.png

BR,
Peter

0 Kudos
Reply

7,415 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @PeterYang_TW ,

 

I sent email to you.  check it, please!

I was a little confused, so we discuss it in email directly.

 

Regards,

weidong

0 Kudos
Reply

7,256 Views
PeterYang_TW
Contributor I

Dear @weidong_sun ,

Do you have any updates about this issue?

BR,
Peter

0 Kudos
Reply

7,247 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @PeterYang_TW ,

 

I have ever sent email to you, did you receive it?

 

Regards,

weidong

0 Kudos
Reply

7,513 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @PeterYang_TW ,

 

Could you help to provide some information I need?

1. Linux kernel version.

2. detailed operation steps, including loading driver.

Note:

This is the latest driver for 8897 , could you try it?

weidong_sun_0-1678876315711.png

https://www.nxp.com/products/wireless/wi-fi-plus-bluetooth-plus-802-15-4/2-4-5-ghz-dual-band-2x2-wi-...

 

Regards,

weidong

0 Kudos
Reply

7,509 Views
PeterYang_TW
Contributor I

Hi @weidong_sun 

Please refer to my following reply.

1. Linux kernel version.
Our Linux version is 4.9.96

2. detailed operation steps, including loading driver.
loading driver -
insmod 8897mlan.ko
insmod sd8897.ko driver host_mlme=1 drvdbg=0x6 cfg80211_wext=0xf sta_name=wlan wfd_name=p2p max_vir_bss=1 drv_mode=7 p2p_enh=1 wakelock_timeout=30  cal_data_cfg=cal_data.conf
insmod mbt8897.ko

operation steps -
1. Connect to 2.4 or 5 GHz AP
2. Connect to BT RCU
3. Press a power key and our android box entered standby. 

This issue can be reproduced with the latest driver SD8897-15.68.19.p59.1-C3X15CS698.p1-GPL-(FP68).

BR,
Peter

0 Kudos
Reply