wifi/bt module with AzureRTOS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

wifi/bt module with AzureRTOS

3,778 Views
Kbrannan
Contributor II

Hello,

I am trying to port a Bluetooth example for use with Azure RTOS, but I am having trouble understanding the architecture of the project. 

I'm developing on the MIMXRT1170-EVKB SDK and currently looking at the  peripheral_ht SDK Example for use with the WIFI_IW416_BOARD_MURATA_1XK_M2 module. 

What is the difference between the Ethermind driver and Edgefast? 

It looks like most of the core is already abstracted using various OS abstraction layers. Can an OSA layers be used to port the entire project over to AzureRTOS? 

0 Kudos
Reply
11 Replies

3,746 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @Kbrannan 

Thanks for creating case to us and hope you are doing well.

I will check it and reply to you once have any updates.

Have a nice weekend.

 

Best regards,

Christine.

Tags (1)
0 Kudos
Reply

3,718 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @Kbrannan 

Please refer to:

SDK_2_15_000_MIMXRT1170-EVKB\middleware\edgefast_bluetooth\source

This subfolder includes EdgeFast Bluetooth Protocol Abstraction Layer host stack source code based on the Ethermind Bluetooth host stack APIs.

EdgeFast Bluetooth PAL (Protocol Abstraction Layer) uses the ethermind stack as lower layer.

Please refer to: 

SDK_2_15_000_MIMXRT1170-EVKB\docs\wireless\bluetooth\edgefast_bluetooth\ 

There is three files related to Edgefast, and to remind you there is some hardware rework for MIMXRT1170-EVKB and Murata 1XK M.2 Adapter, you can refer to: Hardware Rework Guide for EdgeFast BT PAL.pdf.

About AzureRTOS, please refer to Getting Started with MCUXpresso SDK for Azure RTOS.pdf located in the SDK_2_15_000_MIMXRT1170-EVKB\docs\AzureRTOS\.

 

Best regards,

Christine.

Tags (1)
0 Kudos
Reply

3,654 Views
Lizardkomodo
Contributor I

Hi, I just tried to import the edge fast middleware into the ThreadX example, but I cannot select it from the SDK manager, only the wifi example is supported.

 

image.png

0 Kudos
Reply

3,638 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @Lizardkomodo 

Thanks for your reply.

Can you please help to check your SDK version?

Because I am using SDK_2_15_000_MIMXRT1170-EVKB, I can import the edge fast bluetooth middleware into the ThreadX example.

Please see below:

Christine_Li_0-1715410157680.png

And I also checked SDK_2_14_0_MIMXRT1170-EVK, there is even no edgefast_bluetooth folder under middleware.

Christine_Li_1-1715410252609.png

So, please help to check your SDK version, and update it the the latest one to have a try.

Best regards,

Christine.

 

Tags (1)
0 Kudos
Reply

3,609 Views
Lizardkomodo
Contributor I

Thank you I am able to see it now with the updated 1.15 MDK. I loaded a new ThreadX Demo Example and imported the Edgefast Bluetooth middleware into it, it seems like it is missing some dependencies upon building. I am also noticing some calls to zephyr. Does the middleware run on Zephyr RTOS? If so then I do not think this will be suitable for my application, which runs on AzureRTOS.

2024-05-14 10_52_04-.png

.

0 Kudos
Reply

3,565 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @Lizardkomodo 

Thanks for your reply.

I tried on my side locally, but it seems different errors with your side.

Can you please let me know your detailed steps? Like which SDK you are using and, which files did you import to your example?

And are you also using same example(ThreadX_demo) with Kbrannan?

 

Christine_Li_0-1716200146243.png

Please let me know your details, so that I can reproduce on my side, and support you better.

Best regards,

Christine.

Tags (1)
0 Kudos
Reply

3,552 Views
Lizardkomodo
Contributor I

Yes I am using the same example. Here is what I did.

First I open my IDE.

2024-05-20 17_47_35-.png

Then after picking my default workspace I Import an SDK example from the main menu.

2024-05-20 17_49_09-workspace - MCUXpresso IDE.png

I select my board

2024-05-20 17_49_26-workspace - MCUXpresso IDE.png

Then click next to import the threadx example.

2024-05-20 17_49_42-SDK Import Wizard.pngAfter I click on "Finish" the project is in my workspace and I can open it. Now i click on SDK manager to import the middleware.

2024-05-20 18_07_27-.png

From here I select the Edgefast Bluetooth Middleware.

 

2024-05-20 17_50_50-workspace - evkbmimxrt1170_threadx_demo_source_threadx_demo.c - MCUXpresso IDE.png

A prompt asks me this. to which I click "Yes"

2024-05-20 17_51_01-workspace - evkbmimxrt1170_threadx_demo_source_threadx_demo.c - MCUXpresso IDE.png

After it has finished loading, then i click to Build the Project.

2024-05-20 17_53_14-.png

After the project finishes building I receive multiple errors.

2024-05-20 17_53_32-workspace - evkbmimxrt1170_threadx_demo_source_threadx_demo.c - MCUXpresso IDE.png

2024-05-20 17_53_41-workspace - evkbmimxrt1170_threadx_demo_source_threadx_demo.c - MCUXpresso IDE.png

0 Kudos
Reply

3,503 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @Lizardkomodo 

Thanks for the detailed steps.

I think we are using different SDK version. You are using SDK V2.15.100 and I am using SDK V2.15.000.

So to reproduce your issue, I will upgrade the SDK version, then share the updates with you.

 

Best regards,

Christine.

Tags (1)
0 Kudos
Reply

3,486 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @Lizardkomodo 

I reproduced partially your errors.

To solve the problem, I think you need to import the head files from SDK into your workspace.

You can search the file which not found when build, and search the name in your SDK directory, after found the file location, then copy it into your workspace related location.

I am trying on my local side, too.

 

Best regards,

Christine.

Tags (1)
0 Kudos
Reply

3,479 Views
Lizardkomodo
Contributor I

Hi, I am not sure what you mean by the SDK directory, could you please show me how you managed to fix the errors?

0 Kudos
Reply

3,454 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @Lizardkomodo 

Actually I haven't resolved all of the errors on my side.

But there are two ways you can try:

1. According to the errors, copy the needed files from SDK directory to where it requests. I believe you have downloaded our SDK from our website and also imported it to MCUXpresso IDE. You can find where is your SDK, unzip it, and find the needed files by searching the name of related files. But as our experience, directly import the whole edgefast bluetooth middleware to another separate demo example will  encounter a lot of errors. And to resolve these compile errors might take a lot of your time.

2. Do not directly import the whole middleware, but only import what you need and add requested files.

This way might be a better way for whom isn't very familiar with the whole code structure.

Why don't you use our default Demo example and do some customized based on it? 

Actually it has been out our support, to import some middleware to some demo examples. It is customization part of customers.

Best regards,

Christine.

Tags (1)
0 Kudos
Reply