[imx8m] wifi mesh support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[imx8m] wifi mesh support

Jump to solution
2,448 Views
Andy_Lee
Contributor II

I would like to ask wifi mesh support at imx8m evk platform w/ SD8987.

I set it like the following in the menuconfig.
CONFIG_MAC80211_MESH=y

CONFIG_MAC80211_SUPPORT=y
CONFIG_MAC80211_SUPPORT_UAP=y
CONFIG_MAC80211_SUPPORT_MESH=y

But, I did not find any mesh point at target evk board.

Could you explain how to enable wifi mesh point at imx8m evk platform ?

================================================================================
root@imx8mnevk:~# modprobe moal mod_para=nxp/wifi_mod_para.conf
[59069.386690] wlan: Loading MWLAN driver !!!!
[59069.391414] wlan: woal_init_from_dev_tree !!!!
[59069.397172] wlan: Register to Bus Driver...
[59069.401557] vendor=0x02DF device=0x9149 class=0 function=1
[59069.407140] Attach moal handle ops, card interface type: 0x105
[59069.414871] SD8987: init module param from usr cfg
[59069.419710] card_type: SD8987, config block: 0
[59069.424196] cfg80211_wext=0xf
[59069.427188] max_vir_bss=1
[59069.429824] cal_data_cfg=none
[59069.432802] ps_mode = 1
[59069.435249] auto_ds = 1
[59069.437727] host_mlme=enable
[59069.440628] fw_name=nxp/sdiouart8987_combo_v0.bin
[59069.445362] SDIO: max_segs=128 max_seg_size=65535
[59069.450085] rx_work=1 cpu_num=4
[59069.453256] Attach mlan adapter operations.card_type is 0x105.
[59069.459427] wlan: Enable TX SG mode
[59069.462953] wlan: Enable RX SG mode
[59069.472543] Request firmware: nxp/sdiouart8987_combo_v0.bin
[59069.826132] Wlan: FW download over, firmwarelen=595196 downloaded 595196
[59070.698671] WLAN FW is active
[59070.701667] on_time is 59070701271625
[59070.752656] fw_cap_info=0x181d7f03, dev_cap_mask=0xffffffff
[59070.758288] max_p2p_conn = 8, max_sta_conn = 8
[59070.763059] SDIO rx aggr: 1 block_size=512
[59070.767246] wlan: Enable RX SG mode
[59070.770779] mpa_rx_buf_size=65280
[59070.808213] wlan: version = SD8987----16.92.21.p41.3-MM5X16322.p3-(FP92)
[59070.820054] wlan: Register to Bus Driver Done
[59070.824676] wlan: Driver loaded successfully
root@imx8mnevk:~#

root@imx8mnevk:~# ifconfig -a
eth0: flags=4099<UP,BROADCAST,MULTICAST> mtu 1500
ether 00:04:9f:07:11:d8 txqueuelen 1000 (Ethernet)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 0 bytes 0 (0.0 B)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0

lo: flags=73<UP,LOOPBACK,RUNNING> mtu 65536
inet 127.0.0.1 netmask 255.0.0.0
inet6 ::1 prefixlen 128 scopeid 0x10<host>
loop txqueuelen 1000 (Local Loopback)
RX packets 47276 bytes 2886032 (2.7 MiB)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 47276 bytes 2886032 (2.7 MiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0

mlan0: flags=4098<BROADCAST,MULTICAST> mtu 1500
ether 20:4e:f6:d7:b0:87 txqueuelen 1000 (Ethernet)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 0 bytes 0 (0.0 B)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0

uap0: flags=4098<BROADCAST,MULTICAST> mtu 1500
ether 20:4e:f6:d7:b1:87 txqueuelen 1000 (Ethernet)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 0 bytes 0 (0.0 B)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0

wfd0: flags=4098<BROADCAST,MULTICAST> mtu 1500
ether 22:4e:f6:d7:b0:87 txqueuelen 1000 (Ethernet)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 0 bytes 0 (0.0 B)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0

root@imx8mnevk:~# iw dev
phy#0
Interface wfd0
ifindex 5
wdev 0x3
addr 22:4e:f6:d7:b0:87
type managed
txpower 24.00 dBm
Interface uap0
ifindex 4
wdev 0x2
addr 20:4e:f6:d7:b1:87
type AP
txpower 24.00 dBm
Interface mlan0
ifindex 3
wdev 0x1
addr 20:4e:f6:d7:b0:87
type managed
txpower 24.00 dBm
root@imx8mnevk:~#

================================================================================

Best regards
Andy Lee

Labels (2)
0 Kudos
Reply
1 Solution
2,387 Views
Andy_Lee
Contributor II

Hello, NXP TechSupport team.

 

Thank you for your kind help.

We are understanding your situation. Also Accepted your current answer.

 

May I ask you one more time, 

Do you have any update plan of supporting of WiFi Mesh in near future ? 

 

If you have no plan, You can close this topic.

 

Best regards

Andy Lee

View solution in original post

0 Kudos
Reply
4 Replies
2,428 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

 

While the device support several features, some of them might not be enabled in the BSP .

By any chance, which driver are you using for the device ? You can check in this link the different features enabled in the Linux Board Support Packages (BSPs).

Also, if you are not using those drivers, could you please help me validate that in the document of the features of teh driver to validate if the WIFI mesh is mentioned there ?

 

Regards

0 Kudos
Reply
2,422 Views
Andy_Lee
Contributor II

Hello.

I am using driver like as below

---------------------------------------------------------------------------

SD-UART 8987
BSP version : Linux 5.15.32-2.0.0
Wi-Fi and Bluetooth/Bluetooth LE Firmware version : 16.92.21.p41.3
Driver version : MM5X16322.p3-GPL

wlan: version = SD8987----16.92.21.p41.3-MM5X16322.p3-(FP92)

--------------------------------------------------------------------------

BSP support wifi mesh ? or not ? 

if it is not support wifi mesh point at SD8987,  Is it support wifi mesh support at SD/PCIE9098 ?

 

Best regard

Andy Lee

0 Kudos
Reply
2,417 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

I apologize for the inconvenience this might cause you, the driver you are currently using does not include the support of WiFi Mesh .

 

Regards

0 Kudos
Reply
2,388 Views
Andy_Lee
Contributor II

Hello, NXP TechSupport team.

 

Thank you for your kind help.

We are understanding your situation. Also Accepted your current answer.

 

May I ask you one more time, 

Do you have any update plan of supporting of WiFi Mesh in near future ? 

 

If you have no plan, You can close this topic.

 

Best regards

Andy Lee

0 Kudos
Reply