I been having issues building a Yocto image with working wifi and bluetooth. I followed the instructions on the pdf tutorial
Clone the repo and sync:
$ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-mickledore -m imx-6.1.36-2.1.0.xml
$ repo sync
Initialize the build:
$ DISTRO="fsl-imx-wayland" MACHINE="imx8mp-lpddr4-evk" source imx-setup-release.sh -b imx-builds
Build the image (no changes where made into the local.conf file):
$ bitbake imx-image-full
This generated an image with 18 warnings that doesn't seem important, such as:
WARNING: cinematicexperience-rhi-1.0-r0 do_package_qa: QA Issue: File /usr/src/debug/cinematicexperience-rhi/1.0-r0/.rcc/qrc_cinematic-shaders.cpp in package cinematicexperience-rhi-src contains reference to TMPDIR
WARNING: onnxruntime-1.16.1-r0 do_package_qa: QA Issue: File /usr/bin/onnxruntime-1.16.1/tests/onnxruntime_test_all in package onnxruntime-tests contains reference to TMPDIR [buildpaths]
WARNING: qtbase-6.5.0-r0 do_package_qa: QA Issue: File /usr/lib/qtbase/ptest/tests/auto/dbus/qdbusabstractinterface/pinger_interface.h in package qtbase-ptest contains reference to TMPDIR
...
On eMMC mode. I enter the u-boot console and mounted the eMMC memory into my system
u-boot=> ums 0 mmc 2
UMS: LUN 0, dev mmc 2, hwpart 0, sector 0x0, count 0x3a68000
Once mounted it. I flashed the memory with the generated image:
$ zstdcat imx-image-full-imx8mp-lpddr4-evk.wic.zst | sudo dd of=/dev/sdc bs=1M conv=fsync status=progress
8934785024 bytes (8.9 GB, 8.3 GiB) copied, 377 s, 23.7 MB/s8938585088 bytes (8.9 GB, 8.3 GiB) copied, 377.181 s, 23.7 MB/s
Once it booted I enter the root user and tried to enable the wifi module:
$ modprobe moal mod_para=nxp/wifi_mod_para.conf
[ 48.145268] mlan: loading out-of-tree module taints kernel.
[ 48.172891] wlan: Loading MWLAN driver
[ 48.177259] wlan: Register to Bus Driver...
[ 48.181718] wlan_pcie 0000:01:00.0: enabling device (0000 -> 0002)
[ 48.187991] PCI memory map Virt0: 00000000816126a8 PCI memory map Virt2: 0000000003b32c17
[ 48.196219] Attach moal handle ops, card interface type: 0x204
[ 48.202092] rps set to 0 from module param
[ 48.207182] PCIE8997: init module param from usr cfg
[ 48.212315] card_type: PCIE8997, config block: 0
[ 48.217064] cfg80211_wext=0xf
[ 48.220418] max_vir_bss=1
[ 48.223236] cal_data_cfg=none
[ 48.226238] ps_mode = 1
[ 48.228688] auto_ds = 1
[ 48.231160] host_mlme=enable
[ 48.234059] fw_name=nxp/pcieuart8997_combo_v4.bin
[ 48.238793] rx_work=1 cpu_num=4
[ 48.241950] Enable moal_recv_amsdu_packet
[ 48.245985] Attach mlan adapter operations.card_type is 0x204.
[ 48.253868] Request firmware: nxp/pcieuart8997_combo_v4.bin
[ 48.861714] FW download over, size 622824 bytes
[ 49.566289] WLAN FW is active
[ 49.569271] on_time is 49567624625
[ 49.610443] FW country code WW does not match with US
[ 49.615691] fw_cap_info=0x587c7fa3, dev_cap_mask=0xffffffff
[ 49.621295] max_p2p_conn = 8, max_sta_conn = 8
[ 49.636091] Register NXP 802.11 Adapter mlan0
[ 49.640609] wlan: uap%d set max_mtu 2000
[ 49.646391] Register NXP 802.11 Adapter uap0
[ 49.656925] Register NXP 802.11 Adapter wfd0
[ 49.661291] wlan: version = PCIE8997--16.92.21.p84.4-MM6X16423.p6-GPL-(FP92)
[ 49.671821] wlan: Register to Bus Driver Done
[ 49.676455] wlan: Driver loaded successfully
After this I was expecting to see the wifi module loaded but to my surprise is not there
$ ifconfig
eth0: flags=4099<UP,BROADCAST,MULTICAST> mtu 1500
ether 00:04:9f:08:3c:8e txqueuelen 1000 (Ethernet)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 0 bytes 0 (0.0 B)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
eth1: flags=4099<UP,BROADCAST,MULTICAST> mtu 1500
ether 00:04:9f:08:3c:8f txqueuelen 1000 (Ethernet)
RX packets 0 bytes 0 (0.0 B)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 0 bytes 0 (0.0 B)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
device interrupt 222
lo: flags=73<UP,LOOPBACK,RUNNING> mtu 65536
inet 127.0.0.1 netmask 255.0.0.0
inet6 ::1 prefixlen 128 scopeid 0x10<host>
loop txqueuelen 1000 (Local Loopback)
RX packets 104 bytes 8628 (8.4 KiB)
RX errors 0 dropped 0 overruns 0 frame 0
TX packets 104 bytes 8628 (8.4 KiB)
TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0
Why the wifi module is not there? I tried following this guide about wifi modules. The module I have is the AW-CM276MA.
I tried enabling SDIO on M.2 connector by doing:
u-boot=> setenv fdtfile imx8mq-evk-usdhc2-m2.dtb
u-boot=> saveenv
Saving Environment to MMC... Writing to MMC(2)... OK
u-boot=> reset
resetting ...
But when I do that the os doesn't boot anymore.
I checked other post such as:
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-use-Bluetooth-on-i-MX8M-boards/ta...
https://community.nxp.com/t5/i-MX-Processors/How-to-configure-Yocto-to-enable-WiFi-BT-on-the-i-MX8-M...
https://community.nxp.com/t5/i-MX-Processors/Bring-up-wifi-BT-with-Imx8mp-evk-with-yocto-Linux/m-p/1...
I also tried downloading the official demo image from NXP Same thing happens.
Am I missing copy some file?
Do I need to enable something in Yocto?
Do I need to enable something on the kernel config?