Issues with Matter Thermostat Development on Custom Board with RT1060 IW612 (u-blox w276)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issues with Matter Thermostat Development on Custom Board with RT1060 IW612 (u-blox w276)

110 次查看
pooisonner
Contributor III

Hello,

I am developing a Matter thermostat on a custom board using RT1060 + IW612 (u-blox w276).

Matter SDK: Release / V1.4.0 MCU: RT1062CVL5B

Flash: 8MB SDRAM: 16MB

There are two issues:

The first issue is a hard fault occurring during Matter commissioning.

  • The Matter SDK source code has not been modified.
  • On the EVBC, commissioning works fine with the Murata module.
  • However, with the u-blox module using the same IW612 chipset, commissioning fails.

The second issue is related to SE051 integration.

Please provide guidance on these issues.

Thank you.

标记 (1)
0 项奖励
回复
1 回复

72 次查看
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well.  Are you following a guide or document to adapt the example to your specific RT1060 MCU?

What changes did you implement to the matter example?

What changes did you implement the change from different modules? (Even if based on same IW612)

 

The available support for our products is listed here: Release v1.4.0.2.1 · NXP/matter.

 

Regards,

Ricardo

0 项奖励
回复