We are looking for WiFi/BLE module from IW61x / IW41x family to connect with LPC55S28 microcontroller (by SDIo / or SPI .. UART is too slow).
Is there any chance for support such option in NXP MCUXpresso SDK ?
解決済! 解決策の投稿を見る。
Hi,
We don't have support for wireless SoC's with the LPC series. The main reason is due to flash limitation. The FW must be stored in the host so it can be streamed into the SoC (the SoC doesn't have flash which means every time the application boots the fw has to be downloaded). Theoretically, you could store the FW on an external flash, but we don't have any reference code for this.
If you would like to use an embedded flash MCU, MCXN947 could be an option.
By the way, there is an example on the RT1060-EVKB which can use the RW612 as NCP via SDIO, SPI, USB, or UART.
I hope this helps.
Regards,
Daniel.
Hi,
We don't have support for wireless SoC's with the LPC series. The main reason is due to flash limitation. The FW must be stored in the host so it can be streamed into the SoC (the SoC doesn't have flash which means every time the application boots the fw has to be downloaded). Theoretically, you could store the FW on an external flash, but we don't have any reference code for this.
If you would like to use an embedded flash MCU, MCXN947 could be an option.
By the way, there is an example on the RT1060-EVKB which can use the RW612 as NCP via SDIO, SPI, USB, or UART.
I hope this helps.
Regards,
Daniel.
Unfortunately, seems these are the only options we have. If you would like to know more about the NCP app, there is UM12133 available in the RW61x documentation.
I'm sorry for the inconvenience this might cause you.
Regards,
Daniel.