IW610 802.15.4 problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IW610 802.15.4 problems

386 Views
me_nias
Contributor I

Hi,

We are trying to get started with openthread using an IW610G module but having some troubles during the initial SPI communication.

How do I know if the firmware is compatible with 802.15.4? We are using the latets binary (sduartspi_iw610.bin.se, ver: SDIW610---18.99.5.p61-MM6X18505.p7.1-(FP92)) from the nxp-imx/imx-firmware github.

Is there something more that must be done while building ot-daemon than adding the build options? (-DOT_APP_RCP=ON, -DOT_RCP=ON, -DOT_TRANSPORT=spi, -DOT_POSIX_RCP_SPI=ON, DOT_POSIX_RCP_SPI_BUS=ON)

I have attached the system log and a logic analyzer capture of the SPI signals.

Any help is much appreciated,
Cheers!

0 Kudos
Reply
3 Replies

336 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. You can check the Feature Thread list for our different devices here: NXP Wireless SoC Features and Release Notes for Linux

You can check a description of the firmware's on this document: Getting Started with IW610 module on FRDM i.MX 91 development board running Linux OS. Also, I would recommend checking section 11, that is related 802.15.4.

Hope this helps.

 

Best Regards,

Ricardo

Best Regards,
Ricardo
0 Kudos
Reply

190 Views
me_nias
Contributor I

Hi Ricardo,

Thank you for your reply.

I can see from the document RN00104 that iw610 is running FP99. It confuses me however that the feature pack is defined by the second version section, i.e. "99" in 18.99.5.p61, while my driver is outputting "wlan: version = SDIW610---18.99.5.p21-MM6X18505.p7.1-(FP92)". What is "FP92" in this case?

What also confuses me is that the same firmware binary that I am using gives the output "wlan: version = SDIW610---18.99.5.p21-MX6X18475-(FP99)" on a developers kit provided by EmbeddedArtists, where 802.15.4 supposedly works (note the "FP99"). This leads me to think that the feature pack "FP92"/"FP99" is decided also by the linux driver (moal?)?

0 Kudos
Reply

119 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

More information about the SW for Wireless can be found here: Linux Software Reference Manual for NXP Wireless Connectivity

 

Hope this helps!

Regards,

Ricardo

Best Regards,
Ricardo
0 Kudos
Reply