Hi,
I just tested this on my side using NXP i.MX Linux BSP 5.4.70.
Please let me know if you notice any difference in my logs.
root@imx8mpevk:~# uname -r
5.4.70-2.3.0+g4f2631b022d8
root@imx8mpevk:~# modprobe moal mod_para=nxp/wifi_mod_para.conf
[ 29.275496] wlan: Loading MWLAN driver
[ 29.279808] wlan_pcie 0000:01:00.0: enabling device (0000 -> 0002)
[ 29.286118] Attach moal handle ops, card interface type: 0x204
[ 29.292474] PCIE8997: init module param from usr cfg
[ 29.297488] card_type: PCIE8997, config block: 0
[ 29.302137] cfg80211_wext=0xf
[ 29.305105] wfd_name=p2p
[ 29.307659] max_vir_bss=1
[ 29.310294] cal_data_cfg=none
[ 29.313260] drv_mode = 7
[ 29.315807] ps_mode = 2
[ 29.318267] auto_ds = 2
[ 29.320713] fw_name=nxp/pcieuart8997_combo_v4.bin
[ 29.325451] rx_work=1 cpu_num=4
[ 29.328623] Attach mlan adapter operations.card_type is 0x204.
[ 29.338096] Request firmware: nxp/pcieuart8997_combo_v4.bin
[ 30.181883] FW download over, size 551108 bytes
[ 31.050098] WLAN FW is active
[ 31.053073] on_time is 31051009375
[ 31.085072] fw_cap_info=0x181c3fa3, dev_cap_mask=0xffffffff
[ 31.090680] max_p2p_conn = 8, max_sta_conn = 8
[ 31.108982] wlan: version = PCIE8997-16.92.10.p118-MXM5X16210-GPL-(FP92)
[ 31.116074] wlan: Driver loaded successfully
root@imx8mpevk:~# [ 33.758106] can1-stby: disabling
[ 33.761343] can2-stby: disabling
[ 33.764597] VSD_3V3: disabling
root@imx8mpevk:~# hciattach /dev/ttymxc0 any 115200 flow
Setting TTY to N_HCI line discipline
Device setup complete
root@imx8mpevk:~# hciconfig
hci0: Type: Primary Bus: UART
BD Address: CC:47:40:33:61:76 ACL MTU: 1016:5 SCO MTU: 120:6
DOWN
RX bytes:691 acl:0 sco:0 events:38 errors:0
TX bytes:438 acl:0 sco:0 commands:38 errors:0
root@imx8mpevk:~# hciconfig hci0 up
root@imx8mpevk:~# hciconfig
hci0: Type: Primary Bus: UART
BD Address: CC:47:40:33:61:76 ACL MTU: 1016:5 SCO MTU: 120:6
UP RUNNING
RX bytes:1424 acl:0 sco:0 events:82 errors:0
TX bytes:1218 acl:0 sco:0 commands:82 errors:0
root@imx8mpevk:~#
Regards,
Daniel.