Android: Driver/firmware porting/integrating guide of 88w8997

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android: Driver/firmware porting/integrating guide of 88w8997

3,518 Views
Abhijeet_Therokar
Contributor I

Hi NXP team,

We are using the 88w8997 SoC for WIFI and BT in a product running on Android 12.

Is there any driver/firmware porting guide for the same?

We did check it on the official site in a product document section but it is not available.

It will be helpful if you provide us the porting document.

 

We are awaiting to hear from you.

Thanks,

Abhijeet Therokar

0 Kudos
Reply
5 Replies

3,427 Views
Abhijeet_Therokar
Contributor I

Hi @weidong_sun,
Can you share the Porting guide for Android 11?
Also, it will be helpful if you let us know how to verify that driver has been probed using dmesg/logcat.

Thanks,

Abhijeet Therokar

0 Kudos
Reply

3,412 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @Abhijeet_Therokar ,

 

You can refter to the AN for 9098, and port your 8997 to android 11.

I don't have rights to upload files here.  if you have right to access wifi page, you can download it.

=============================

https://www.nxp.com/products/wireless/wi-fi-plus-bluetooth-plus-802-15-4/2-4-5-ghz-dual-band-2x2-wi-...
--->AN - 88Q9098-88W9098 - Android Vendor HAL v009 Integration Guide

weidong_sun_0-1678149398717.png

 

--->Android_Vendor_HAL_M009.008_M009.013

weidong_sun_0-1678149495843.png

 

 

===============================

Regards,

weidong

0 Kudos
Reply

3,415 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @Abhijeet_Therokar ,

 

You can refter to the AN for 9098, and port your 8997 to android 11.

I don't have rights to upload files here.  if you have right to access wifi page, you can download it.

=============================

https://www.nxp.com/products/wireless/wi-fi-plus-bluetooth-plus-802-15-4/2-4-5-ghz-dual-band-2x2-wi-...
--->AN - 88Q9098-88W9098 - Android Vendor HAL v009 Integration Guide

weidong_sun_0-1678149398717.png

 

--->Android_Vendor_HAL_M009.008_M009.013

weidong_sun_1-1678149426140.png

 

===============================

Regards,

weidong

0 Kudos
Reply

3,495 Views
Abhijeet_Therokar
Contributor I

Hi @weidong_sun,
Thanks for the detailed explanation.

BR,

Abhijeet Therokar

0 Kudos
Reply

3,501 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Dear @Abhijeet_Therokar ,

1. Getting driver & firmware

#git clone http://source.codeaurora.org/external/imx/mwifiex.git

#cd mwifiex

# git tag

android-11.0.0_2.0.0
android-11.0.0_2.2.0
android-11.0.0_2.2.0-imx8ulp-er
android-11.0.0_2.4.0
android-11.0.0_2.6.0
android-12.0.0_1.0.0
android-12.0.0_2.0.0
automotive-11.0.0_2.1.0
automotive-11.0.0_2.3.0
automotive-11.0.0_2.5.0
automotive-12.0.0_1.1.0
lf-5.10.35-2.0.0
lf-5.10.52-2.1.0
lf-5.10.72-2.2.0
lf-5.10.72-2.2.2
lf-5.10.y-1.0.0
lf-5.15.32-2.0.0
lf-5.15.5-1.0.0
rel_imx_5.4.24_2.1.0
rel_imx_5.4.47_2.2.0
rel_imx_5.4.70_2.3.0
rel_imx_5.4.70_2.3.2

# git checkout android-12.0.0_2.0.0

(Assume you are using android-12.0.0_2.0.0)

2. firmware & wifi_mod_para.conf

According to your kernel version, download firmware. Assume you are using 5.10.72

https://github.com/nxp-imx/imx-firmware/tree/lf-5.10.72_2.2.0/nxp

weidong_sun_0-1676950030872.png

3. WiFi & BT HAL 

By default , Our i.MX android 12 BSP supports 8997. you can use the WiFi HAL & BT HAL if you are not using i.MX platform.

weidong_sun_1-1676950198045.png

you can download our android 12 source code & bsp, then get it. 

4. no porting guide for android 12. But android 11.

 

Regards,

weidong

0 Kudos
Reply