Hi, Andy, After download our Driver package, you can directly compile with "make build" command without any modification in Makefile.
It can be built successfully if you are using Ubuntu 20.04 Linux.
Please try this Driver: PCIE-WLAN-UART-BT-8997-U16-X86-16.92.21.p55.3-16.92.21.p55.3-MM5X16344.P3-MGPL
This driver code supports Linux kernel from 2.6.32 to 5.15.
You can find it on our website after log in.
Kindly remind: after log in, click "Design Resources",Choose "Software" and click "Secure Files" then click "Show all" button. image.png I also attach the download link below for your convenience.
I have tested it and made successfully on my local side(Ubuntu 20.04 on X86 platform)
https://www.nxp.com/webapp/sps/download/license.jsp?colCode=PCIE-WLAN.UART_BT_8997_U16.X86_MM5X16344...
For more build info details you can also see the README file in our driver package under WIFI-BT-U16-X86--MM5X17344.p3-MGPL/wlan_src directory after decompress it.
Above driver is not the latest one, but also new released this year(Sep 29, 2022).
The latest driver(PCIE-WLAN-UART-BT-8997-LNX_5_15_71-IMX8-16.92.21.p55.3-16.92.21.p55.3-MM5X16366.P5-MGPL ) download link is shown as below:
https://www.nxp.com/webapp/sps/download/license.jsp?colCode=PCIE-8997-LNX.5.15.71.p55.3-MM5X16366.P5...
Best regards,
Christine.