vybrid processor ADC ADC_HS COCO( conversion complete) bit is not going high for first 10 milliseconds

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

vybrid processor ADC ADC_HS COCO( conversion complete) bit is not going high for first 10 milliseconds

965件の閲覧回数
damodaranmurthy
Contributor I

vybrid processor ADC ADC_HS COCO( conversion complete) bit is not going high for first 10 milliseconds , after 10ms reinitialized and working fine. ADC read called for every one milliseconds,ADC config details: 12bit, ADIV/8, no low power , 16samples avg, normal speed , software trigger. ADC_init() called once at power up and later for ADC errors same ADC_init called again to reset.

0 件の賞賛
返信
1 返信

810件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

Could you please specify which specific Vybrid part are you using? Additionally, are you using bare-metal code or any other BSP?

Best regards!

/Carlos

0 件の賞賛
返信