vybrid Processor Expert selects multiple pins for I2C0 SCL

cancel
Showing results for 
Search instead for 
Did you mean: 

vybrid Processor Expert selects multiple pins for I2C0 SCL

Jump to solution
1,614 Views
alanball
Contributor III

Hi Guys

I'm using Processor Expert 10.4 to configure a Vybrid

Problem I have is that when I select pin B14 for I2C0 SCL, the tool also checks pins K18 and L3 (which I need for other things)  -see attachment

i2C1 behaves as I would expect (I can select any one of the available pins)

Is this a bug in the tool, or is there some strange dependency in the chip I'm not aware of ?

Labels (2)
0 Kudos
1 Solution
1,366 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
4 Replies
1,367 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
1,369 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I have the same behavior as Vilem.

The version I have is the next:

pastedImage_0.png

I wonder if there is any difference. I am not sure if there is an update package you need.

The installation details are the next:

pastedImage_1.png

Regards,

Alejandro

1,370 Views
alanball
Contributor III

Hi Alejandro & Vilem

Thanks for your reply :smileyhappy:

It looks like there is a later version of PE - I will check

In the meantime, since I was still able to change my hardware design, I changed from I2C0 to I2C1, which does not have any issue

Regards

Alan

0 Kudos
1,370 Views
VilemZ
NXP Employee
NXP Employee

Hi Alan,

I tried select only pin B14 on PEx in new project and it was work. I attaching screen. I think, that i can be affected by other things.

Best Regards

Vilem