vybrid Processor Expert selects multiple pins for I2C0 SCL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

vybrid Processor Expert selects multiple pins for I2C0 SCL

ソリューションへジャンプ
4,963件の閲覧回数
alanball
Contributor III

Hi Guys

I'm using Processor Expert 10.4 to configure a Vybrid

Problem I have is that when I select pin B14 for I2C0 SCL, the tool also checks pins K18 and L3 (which I need for other things)  -see attachment

i2C1 behaves as I would expect (I can select any one of the available pins)

Is this a bug in the tool, or is there some strange dependency in the chip I'm not aware of ?

ラベル(2)
0 件の賞賛
返信
1 解決策
4,715件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,716件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
4,718件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I have the same behavior as Vilem.

The version I have is the next:

pastedImage_0.png

I wonder if there is any difference. I am not sure if there is an update package you need.

The installation details are the next:

pastedImage_1.png

Regards,

Alejandro

4,719件の閲覧回数
alanball
Contributor III

Hi Alejandro & Vilem

Thanks for your reply :smileyhappy:

It looks like there is a later version of PE - I will check

In the meantime, since I was still able to change my hardware design, I changed from I2C0 to I2C1, which does not have any issue

Regards

Alan

0 件の賞賛
返信
4,719件の閲覧回数
VilemZ
NXP Employee
NXP Employee

Hi Alan,

I tried select only pin B14 on PEx in new project and it was work. I attaching screen. I think, that i can be affected by other things.

Best Regards

Vilem