mcc_recv_nocopy never timeouts

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mcc_recv_nocopy never timeouts

1,168 Views
kubiznak_petr
Contributor V

I think I hit on a bug in implementation of blocking calls in MCC library. I'm using mcc_recv_nocopy() with finite non-zero timeout to receive a message from Linux (A5) to MQX (M4) on Vybrid. It works fine if the system time is not changed, but when I change it using the following code, subsequent calls to mcc_recv_nocopy() never return until a message is received (which may never happen).

  _rtc_set_time_mqxd(pDate);

  _rtc_sync_with_mqx(TRUE);

Am I misusing something or is this a bug? Is there any patch? It is pretty important to me.

(I'm not even asking what would happen if I changed the system time between a call to mcc_recv_nocopy() and its return.)

Labels (3)
Tags (5)
2 Replies

546 Views
juangutierrez
NXP Employee
NXP Employee

Would you have a simple test, so I can reproduce the issue at my side?

0 Kudos

546 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi ,

I noticed that the above functions are no longer in the MQX 4.1 version. They are removed and the way to synchronize the RTC with the MQX time is different now.

I am trying to reproduce the problem with MQX 4.1 but it is not failing. One thing I noticed is that if you set a timeout and sometimes fail other does not, after a few seconds both cores stop executing the tasks.

I used the below code, it is the same one found in the mcc/examples folder of  MQX.

This happens no matter if the rtc is used or not.

/*HEADER**********************************************************************

*

* Copyright 2013 Freescale Semiconductor, Inc.

*

* This software is owned or controlled by Freescale Semiconductor.

* Use of this software is governed by the Freescale MQX RTOS License

* distributed with this Material.

* See the MQX_RTOS_LICENSE file distributed for more details.

*

* Brief License Summary:

* This software is provided in source form for you to use free of charge,

* but it is not open source software. You are allowed to use this software

* but you cannot redistribute it or derivative works of it in source form.

* The software may be used only in connection with a product containing

* a Freescale microprocessor, microcontroller, or digital signal processor.

* See license agreement file for full license terms including other

* restrictions.

*****************************************************************************

*

* Comments:

*

*   This file contains the source for one of the MCC pingpong examples.

*

*

*END************************************************************************/

#include <mqx.h>

#include <bsp.h>

#include "mcc.h"

#include "mcc_config.h"

#include "mcc_common.h"

#include "mcc_api.h"

#include "mcc_mqx.h"

#include <string.h>

#include <core_mutex.h>

  DATE_STRUCT   date;

  uint32_t      u32time;

  TIME_STRUCT     mqx_time;

#if ! BSPCFG_ENABLE_IO_SUBSYSTEM

#error This application requires BSPCFG_ENABLE_IO_SUBSYSTEM defined non-zero in user_config.h. Please recompile BSP with this option.

#endif

#ifndef BSP_DEFAULT_IO_CHANNEL_DEFINED

#error This application requires BSP_DEFAULT_IO_CHANNEL to be not NULL. Please set corresponding BSPCFG_ENABLE_TTYx to non-zero in user_config.h and recompile BSP with this option.

#endif

/* Application-specific settings */

/* 1: Blocking mode (task is blocked when no new message is available)

* 0: Non-blocking mode (task is waiting for a new message in a spin loop) */

#define MCC_APP_BLOCKING_MODE  (1)

extern void main_task(uint32_t);

extern void responder_task(uint32_t);

#if PSP_MQX_CPU_IS_VYBRID_A5

const TASK_TEMPLATE_STRUCT  MQX_template_list[] =

{

   /* Task Index,    Function,       Stack,  Priority, Name,        Attributes,          Param, Time Slice */

    { MAIN_TTN,      main_task,      2000,   9,        "Main",      MQX_AUTO_START_TASK, MCC_MQX_NODE_A5,   0 },

    { 0 }

};

#else

TASK_TEMPLATE_STRUCT  MQX_template_list[] =

{

   /* Task Index,    Function,       Stack,  Priority,  Name,        Attributes,          Param, Time Slice */

    { RESPONDER_TTN, responder_task, 2000,   9,         "Responder", MQX_AUTO_START_TASK, MCC_MQX_NODE_M4,  0 },

    { 0 }

};

#endif

MCC_ENDPOINT    mqx_endpoint_a5 = {0,MCC_MQX_NODE_A5,MCC_MQX_SENDER_PORT};

MCC_ENDPOINT    mqx_endpoint_m4 = {1,MCC_MQX_NODE_M4,MCC_MQX_RESPONDER_PORT};

/*TASK*----------------------------------------------------------

*

* Task Name : main_task

* Comments  :

*     This task creates a message pool and a message queue then

*     sends a message to a queue on the second CPU.

*     It waits for a return message, validating the message before

*     sending a new message.

*END*-----------------------------------------------------------*/

void main_task(uint32_t node_num)

{

 

    DATE_STRUCT   date;

    THE_MESSAGE     msg;

    MCC_MEM_SIZE    num_of_received_bytes;

    CORE_MUTEX_PTR  coremutex_app_ptr;

    MCC_INFO_STRUCT mcc_info;

    int             ret_value;

#if !MCC_APP_BLOCKING_MODE

    unsigned int    num_available_msgs;

#endif

    /* create core mutex used in the app. for accessing the serial console */

    coremutex_app_ptr = _core_mutex_create( 0, MCC_PRINTF_SEMAPHORE_NUMBER, MQX_TASK_QUEUE_FIFO );

    msg.DATA = 1;

    ret_value = mcc_initialize(node_num);

    ret_value = mcc_get_info(node_num, &mcc_info);

    if(MCC_SUCCESS == ret_value && (strcmp(mcc_info.version_string, MCC_VERSION_STRING) != 0)) {

        _core_mutex_lock(coremutex_app_ptr);

        printf("\n\n\nError, attempting to use different versions of the MCC library on each core! Application is stopped now.\n");

        _core_mutex_unlock(coremutex_app_ptr);

        mcc_destroy(node_num);

        _task_block();

    }

    ret_value = mcc_create_endpoint(&mqx_endpoint_a5, MCC_MQX_SENDER_PORT);

    _core_mutex_lock(coremutex_app_ptr);

    printf("\n\n\nMain task started, MCC version is %s\n", mcc_info.version_string);

    _core_mutex_unlock(coremutex_app_ptr);

   

    date.YEAR   = 2014;

    date.MONTH  = 3;

    date.DAY    = 5;

    date.HOUR   = 8;

    date.MINUTE = 7;

    date.SECOND = 6;

    date.MILLISEC = 5;

  

   _time_from_date(&date, &mqx_time);

   

   

    _time_get(&mqx_time);

    u32time =  mqx_time.SECONDS ;

    _rtc_set_time(u32time);

     //(void)_rtc_sync_with_mqx(TRUE);

   

   

    while (1) {

        /* wait until the remote endpoint is created by the other core */

        while(MCC_ERR_ENDPOINT == mcc_send(&mqx_endpoint_m4, &msg, sizeof(THE_MESSAGE), 0xffffffff)) {

            _time_delay(1);

        }

#if MCC_APP_BLOCKING_MODE

        ret_value = mcc_recv_copy(&mqx_endpoint_a5, &msg, sizeof(THE_MESSAGE), &num_of_received_bytes, 1000000); //0xffffffff

#else

        mcc_msgs_available(&mqx_endpoint_a5, &num_available_msgs);

        while(num_available_msgs==0) {

            mcc_msgs_available(&mqx_endpoint_a5, &num_available_msgs);

        }

        ret_value = mcc_recv_copy(&mqx_endpoint_a5, &msg, sizeof(THE_MESSAGE), &num_of_received_bytes, 0);

#endif

        if(MCC_SUCCESS != ret_value) {

            _core_mutex_lock(coremutex_app_ptr);

            printf("Main task receive error: %i\n", ret_value);

            _core_mutex_unlock(coremutex_app_ptr);

        } else {

            _core_mutex_lock(coremutex_app_ptr);

            printf("Main task received a msg\n");

            printf("Message: Size=%x, DATA = %x\n", num_of_received_bytes, msg.DATA);

            _core_mutex_unlock(coremutex_app_ptr);

            msg.DATA++;

        }

    }

}

/*TASK*----------------------------------------------------------

*

* Task Name : responder_task

* Comments  :

*     This task creates a message queue then waits for a message.

*     Upon receiving the message the data is incremented before

*     the message is returned to the sender.

*END*-----------------------------------------------------------*/

void responder_task(uint32_t node_num)

{

    THE_MESSAGE     msg;

    MCC_MEM_SIZE    num_of_received_bytes;

    CORE_MUTEX_PTR  coremutex_app_ptr;

    MCC_INFO_STRUCT mcc_info;

    int             ret_value;

#if !MCC_APP_BLOCKING_MODE

    unsigned int    num_available_msgs;

#endif

    /* create core mutex used in the app. for accessing the serial console */

    coremutex_app_ptr = _core_mutex_create( 0, MCC_PRINTF_SEMAPHORE_NUMBER, MQX_TASK_QUEUE_FIFO );

    msg.DATA = 1;

    ret_value = mcc_initialize(node_num);

    ret_value = mcc_get_info(node_num, &mcc_info);

    if(MCC_SUCCESS == ret_value && (strcmp(mcc_info.version_string, MCC_VERSION_STRING) != 0)) {

        _core_mutex_lock(coremutex_app_ptr);

        printf("\n\n\nError, attempting to use different versions of the MCC library on each core! Application is stopped now.\n");

        _core_mutex_unlock(coremutex_app_ptr);

        mcc_destroy(node_num);

        _task_block();

    }

    ret_value = mcc_create_endpoint(&mqx_endpoint_m4, MCC_MQX_RESPONDER_PORT);

    _core_mutex_lock(coremutex_app_ptr);

    printf("\n\n\nResponder task started, MCC version is %s\n", mcc_info.version_string);

    _core_mutex_unlock(coremutex_app_ptr);

    date.YEAR   = 2014;

    date.MONTH  = 3;

    date.DAY    = 5;

    date.HOUR   = 8;

    date.MINUTE = 7;

    date.SECOND = 6;

    date.MILLISEC = 5;

   // _rtc_set_time(&date);

   

   

   // _time_from_date(&date, &mqx_time);

   

   

    //_time_get(&mqx_time);

    //u32time =  mqx_time.SECONDS ;

    //_rtc_set_time(u32time);

     //(void)_rtc_sync_with_mqx(TRUE);   

   

    while (TRUE) {

#if MCC_APP_BLOCKING_MODE

        ret_value = mcc_recv_copy(&mqx_endpoint_m4, &msg, sizeof(THE_MESSAGE), &num_of_received_bytes, 0xffffffff); //0xffffffff

#else

        mcc_msgs_available(&mqx_endpoint_m4, &num_available_msgs);

        while(num_available_msgs==0) {

            mcc_msgs_available(&mqx_endpoint_m4, &num_available_msgs);

        }

        ret_value = mcc_recv_copy(&mqx_endpoint_m4, &msg, sizeof(THE_MESSAGE), &num_of_received_bytes, 0);

#endif

        if(MCC_SUCCESS != ret_value) {

            _core_mutex_lock(coremutex_app_ptr);

            printf("Responder task receive error: %i\n", ret_value);

            _core_mutex_unlock(coremutex_app_ptr);

        } else {

            _core_mutex_lock(coremutex_app_ptr);

            printf("Responder task received a msg\n");

            printf("Message: Size=%x, DATA = %x\n", num_of_received_bytes, msg.DATA);

            _core_mutex_unlock(coremutex_app_ptr);

            msg.DATA++;

            _time_delay(1000);

            ret_value = mcc_send(&mqx_endpoint_a5, &msg, sizeof(THE_MESSAGE), 0xffffffff);

        }

    }

}