hwclock issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hwclock issue

Jump to solution
2,334 Views
Nouchi
Senior Contributor II

Hello Timesys team,

Since I updated the factory (from 20131105 to 20141006), the board lose an hour each time it reboots.

The timezone file still the same (Europe/Paris), and the RTC battery is about 3.0V.

According to the S06-hwclock script, hwclock is started like this: hwclock --systz --localtime

and stopped like that: hwclock --systohc

What can be done to solve this?

Regards,

Emmanuel

Labels (5)
0 Kudos
Reply
1 Solution
1,963 Views
timesyssupport
Senior Contributor II

Hello Nouchi,

What Vybrid platform are you working with? If this is Vybrid Tower Module - what revision of the hardware are you using? Once we know this information, we can better determine what may have changed. Is it correct to assume time was kept correctly before you updated?

There is a known hardware bug with the RTC on older Vybrid Tower modules, as described here:

https://community.freescale.com/message/343277#343277

You have also commented on the above thread - so you are likely already familiar.

Regards,

Timesys Support

View solution in original post

0 Kudos
Reply
4 Replies
1,964 Views
timesyssupport
Senior Contributor II

Hello Nouchi,

What Vybrid platform are you working with? If this is Vybrid Tower Module - what revision of the hardware are you using? Once we know this information, we can better determine what may have changed. Is it correct to assume time was kept correctly before you updated?

There is a known hardware bug with the RTC on older Vybrid Tower modules, as described here:

https://community.freescale.com/message/343277#343277

You have also commented on the above thread - so you are likely already familiar.

Regards,

Timesys Support

0 Kudos
Reply
1,963 Views
Nouchi
Senior Contributor II

Hello,

The platform is our own board based on Vybrid Tower Module, the silicon mask revision is 2N02G, one of the newest.

Weird, since I rebuilt the RFS, it works again.

Thanks

0 Kudos
Reply
1,963 Views
jamesbone
NXP TechSupport
NXP TechSupport

Great to hear! :smileywink:.

1,963 Views
jiri-b36968
NXP Employee
NXP Employee

Hi timesyssupport,

please look at it.
/Jiri

0 Kudos
Reply