hwclock issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,313件の閲覧回数
Nouchi
Senior Contributor II

Hello Timesys team,

Since I updated the factory (from 20131105 to 20141006), the board lose an hour each time it reboots.

The timezone file still the same (Europe/Paris), and the RTC battery is about 3.0V.

According to the S06-hwclock script, hwclock is started like this: hwclock --systz --localtime

and stopped like that: hwclock --systohc

What can be done to solve this?

Regards,

Emmanuel

ラベル(5)
0 件の賞賛
返信
1 解決策
1,942件の閲覧回数
timesyssupport
Senior Contributor II

Hello Nouchi,

What Vybrid platform are you working with? If this is Vybrid Tower Module - what revision of the hardware are you using? Once we know this information, we can better determine what may have changed. Is it correct to assume time was kept correctly before you updated?

There is a known hardware bug with the RTC on older Vybrid Tower modules, as described here:

https://community.freescale.com/message/343277#343277

You have also commented on the above thread - so you are likely already familiar.

Regards,

Timesys Support

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,943件の閲覧回数
timesyssupport
Senior Contributor II

Hello Nouchi,

What Vybrid platform are you working with? If this is Vybrid Tower Module - what revision of the hardware are you using? Once we know this information, we can better determine what may have changed. Is it correct to assume time was kept correctly before you updated?

There is a known hardware bug with the RTC on older Vybrid Tower modules, as described here:

https://community.freescale.com/message/343277#343277

You have also commented on the above thread - so you are likely already familiar.

Regards,

Timesys Support

0 件の賞賛
返信
1,942件の閲覧回数
Nouchi
Senior Contributor II

Hello,

The platform is our own board based on Vybrid Tower Module, the silicon mask revision is 2N02G, one of the newest.

Weird, since I rebuilt the RFS, it works again.

Thanks

0 件の賞賛
返信
1,942件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Great to hear! :smileywink:.

1,942件の閲覧回数
jiri-b36968
NXP Employee
NXP Employee

Hi timesyssupport,

please look at it.
/Jiri

0 件の賞賛
返信