hwclock issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

hwclock issue

跳至解决方案
2,387 次查看
Nouchi
Senior Contributor II

Hello Timesys team,

Since I updated the factory (from 20131105 to 20141006), the board lose an hour each time it reboots.

The timezone file still the same (Europe/Paris), and the RTC battery is about 3.0V.

According to the S06-hwclock script, hwclock is started like this: hwclock --systz --localtime

and stopped like that: hwclock --systohc

What can be done to solve this?

Regards,

Emmanuel

标签 (5)
0 项奖励
回复
1 解答
2,016 次查看
timesyssupport
Senior Contributor II

Hello Nouchi,

What Vybrid platform are you working with? If this is Vybrid Tower Module - what revision of the hardware are you using? Once we know this information, we can better determine what may have changed. Is it correct to assume time was kept correctly before you updated?

There is a known hardware bug with the RTC on older Vybrid Tower modules, as described here:

https://community.freescale.com/message/343277#343277

You have also commented on the above thread - so you are likely already familiar.

Regards,

Timesys Support

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,017 次查看
timesyssupport
Senior Contributor II

Hello Nouchi,

What Vybrid platform are you working with? If this is Vybrid Tower Module - what revision of the hardware are you using? Once we know this information, we can better determine what may have changed. Is it correct to assume time was kept correctly before you updated?

There is a known hardware bug with the RTC on older Vybrid Tower modules, as described here:

https://community.freescale.com/message/343277#343277

You have also commented on the above thread - so you are likely already familiar.

Regards,

Timesys Support

0 项奖励
回复
2,016 次查看
Nouchi
Senior Contributor II

Hello,

The platform is our own board based on Vybrid Tower Module, the silicon mask revision is 2N02G, one of the newest.

Weird, since I rebuilt the RFS, it works again.

Thanks

0 项奖励
回复
2,016 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Great to hear! :smileywink:.

2,016 次查看
jiri-b36968
NXP Employee
NXP Employee

Hi timesyssupport,

please look at it.
/Jiri

0 项奖励
回复