how to disable cache, ESDHC card

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

how to disable cache, ESDHC card

跳至解决方案
2,191 次查看
MehmetAliIpin
Contributor V

Hello,

I could finally download my application into our prototype board's QSPI XIP flashes, and started debugging the code with DS-5. During debug, I saw that boot  code is enabling/disabling cache. And also checking the ESDHC. But we are using VF3x processor, which has no chache in it. Also we don't have SD card in our prototype.

How can I disable these peripherals? in user_config.h?

thanks and best regards.

Mehmet Ali Ipin

标签 (4)
1 解答
1,826 次查看
timesyssupport
Senior Contributor II

Hi Mehmet,

Setting MQX_USE_UNCACHED_MEM to 1 will make MQX compile in support for uncached memory allocation. I also found some cache-related settings at mqx/source/psp/cortex_a/vybrid.h, lines 73-109 (this is for running MQX on either the A5 or M4 core).

Thanks,

Timesys Support

在原帖中查看解决方案

0 项奖励
回复
6 回复数
1,826 次查看
timesyssupport
Senior Contributor II

Hi Mehmet,

Are you looking to disable ESDHC/cache in MQX, Linux, or both? With MQX, you should be able to disable ESDHC in user_config.h. With Linux, the latest kernel checks to see if L2 cache is present before attempting to use it. L2 cache can otherwise be disabled in the kernel configuration. ESDHC support can be disabled in the board definition file, at arch/arm/mach-mvf/board-twr-vf700.c in the Linux source tree.

Thanks, and let me know if you have any questions.

Timesys Support

1,826 次查看
MehmetAliIpin
Contributor V

Hi,

I am looking to disable both ESDHC and cache in MQX.

I guess I should re-set the (#define BSPCFG_ENABLE_ESDHC      1)  to zero;

I only find letter "cache" in line

#define MQX_USE_UNCACHED_MEM     1

Is it this to disable cash, or  are there other lines?

Thanks and best regards.

Mehmet Ali Ipin

0 项奖励
回复
1,827 次查看
timesyssupport
Senior Contributor II

Hi Mehmet,

Setting MQX_USE_UNCACHED_MEM to 1 will make MQX compile in support for uncached memory allocation. I also found some cache-related settings at mqx/source/psp/cortex_a/vybrid.h, lines 73-109 (this is for running MQX on either the A5 or M4 core).

Thanks,

Timesys Support

0 项奖励
回复
1,826 次查看
MehmetAliIpin
Contributor V

Dear Timesys,

I know VF3x has no L2 cache, but in ref manual table 2-4, I read A5 has L1 cache, does it mean data and code caches are available in VF3x? In this case I should only close L2 cache is that true?

#define PSP_HAS_L2_CACHE            0

Thanks and best regards

0 项奖励
回复
1,826 次查看
timesyssupport
Senior Contributor II

Hi Mehmet,

If you are running MQX on the A5 core, then the L1 and L2 cache will be enabled by default, according to mqx/source/psp/cortex_a/vybrid.h, lines 78-84. I am unsure if these are directly related to data/code cache, but changing any of the cache-related macros to 0 in vybrid.h will disable their functionality.

Thanks,

Timesys Support

0 项奖励
回复
1,826 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you attend this case?

0 项奖励
回复