fast ADC conversion for more than one channel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

fast ADC conversion for more than one channel

ソリューションへジャンプ
2,796件の閲覧回数
heinzroitner
Contributor II


Hi Rene Kolarik,

I would like to continue the discussion of thread 329507. We are looking for a fast sample conversion on the internal ADC for 8 channels (for the history of this problem please see threads 317871 and 328250).  Previous implementations using LWADC were either very slow

(450 us) or they did not give 8 different samples.

So we implemented a solution along the description in thread 329507 which is fast and gives different samples. But the debugger shows all kinds of strange behavior as soon as more than one channel is converted.

So the question is: is MQX somehow affected when more channels are converted ? If yes, can you think of another way of implementation ?

Our ISR is:

void iADC_ISR (void * adc_ch)

{

// get last sample

ADC_MemMapPtr adc_ptr = adc_base[current_conv_ch];

uint32_t temp = adc_ptr->R1;

temp = temp & ADC_CDR_CDATA_MASK;

g_iADC0_values[current_conv_ch] = (float)(temp);

// start next conversion

current_conv_ch = (current_conv_ch + 1) % noChannels;

if (current_conv_ch == 0)

{

// stop sampling

}

else

{

adc_ptr = adc_base[current_conv_ch];

uint_32 channel = ADC_CHANNEL(inputs[current_conv_ch]);

adc_base[current_conv_ch]->HC1 = channel | (1 << ADC_HC1_AIEN1_SHIFT);

}

}

We are using the twrvf65gs10 BSP.

Thanks, Heinz

ラベル(3)
0 件の賞賛
返信
1 解決策
2,370件の閲覧回数
rendy
NXP Employee
NXP Employee

Hi, first idea - why do you use floats in interrupt handler? Is it really needed? Can it be the source of the problems?

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
2,371件の閲覧回数
rendy
NXP Employee
NXP Employee

Hi, first idea - why do you use floats in interrupt handler? Is it really needed? Can it be the source of the problems?

0 件の賞賛
返信
2,370件の閲覧回数
heinzroitner
Contributor II

Hi,

OK thanks this is an error in the ISR above. It looks better now after a few runs.

But I have to test it more and in the full program version. I'll tell you then.

Heinz

0 件の賞賛
返信
2,370件の閲覧回数
heinzroitner
Contributor II

Hi Rene,

yes, all the problems were caused by the premature casting of ADC-values to 'float' in the ISR. This gave us much pain.

I thank you for your help and hope you can assist us next time when we are stuck.

Best regards,

Heinz

0 件の賞賛
返信
2,370件の閲覧回数
rendy
NXP Employee
NXP Employee

I'm glad I could help you, just mark my answer as 'Correct' please.

Thanks

Rene

0 件の賞賛
返信
2,370件の閲覧回数
heinzroitner
Contributor II

Hi Rene,

do you also have an explanation what happened here? This would be helpful.

Thanks, Heinz


0 件の賞賛
返信
2,370件の閲覧回数
rendy
NXP Employee
NXP Employee

Hi,

I will check this with MQX team. There is a section in Vybrid Reference Manual - 37.8.5.6 "Conversion Time Examples" - you can check your time constraints there. If it meets your needs, then there will be probably bottleneck in the MQX. I'll be back as soon as I have more info from MQX team.

Rene

0 件の賞賛
返信
2,370件の閲覧回数
heinzroitner
Contributor II

Hi,

the time between ISRs (i.e time needed for one channel conversion) is 8 us. High speed conversion is enabled. So this looks OK.

One type of strange debugger behavior is the overwrite of a certain variable with floating numbers ending in ..E-42. Can you make sense of this? Somehow this must sneak in from the interrrupt ?

Thanks, Heinz

0 件の賞賛
返信
2,370件の閲覧回数
rendy
NXP Employee
NXP Employee

I've just wrote a post about floats below (Oct 1, 2014 11:43 AM). Is it possible for you to defer float processing out of the interrupt context? Aren't there problems with saving of float registers?

0 件の賞賛
返信