chip configuration information: Where is it?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

chip configuration information: Where is it?

跳至解决方案
4,383 次查看
markwatson
Contributor III

IN the Reference Manual there are several places with statements like this:

RXFIFOSIZE field: The reset value depends on whether the specific UART instance supports the FIFO and on the size of

that FIFO. See the Chip Configuration details for more information on the FIFO size supported for each

UART instance.

Where is this information?  I have looked in the Data Sheet, Reference Manual and the Fact sheet.  In several places one can find the number of UARTS, but not the really specific information such as FIFO sizes.

Thanks.

标签 (1)
0 项奖励
回复
1 解答
3,889 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,890 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
回复
3,891 次查看
jiri-b36968
NXP Employee
NXP Employee

Hello Mark,

it is in Chapter 3: Chip Configuration.

Each IP (UART, SPI, DMA, ....) can support different configuration and it depends on the SoC design how it is configured. This chapter include those details.

/Jiri