Dear Naoum,
I apologize for the delay in notifying you.
In EXIT of LPSTOP3, I confirmed that I could correct movement of self_refresh exit of LPDDR2.
In self_refresh exit of LPDDR2, the following processing reaches.
DDRMC->CR35 = DDRMC_CR35_LP_CMD(0x1);
-------------------------------------------------------
I have a question.
It is a rare case, When I leave LPSTOP2, MCU may be hung up.
State at the time of the hangup
・BCTRL signal changes in Low → Hi.
・Exit handling of including the setting GPIO is completed.
・CKE of the DDR is a state of L
I seem to be hung up in SelfRefresh EXIT.
Q1)Should I do WAIT after the following processing?
If I do WAIT, Which time is suitable?
DDRMC->CR35 = DDRMC_CR35_LP_CMD(0x1);
Q2)Please give me advice to be settled.
Best Regards,
soichi