Hi,
I ask about VIU in VF6xx.
I use ITU656 8bit.
Q )
Please teach the following specifications
・Data clock speed to support
・Frame rate to support
・The number of the pixels
Best Regards,
soichi
I have not tested this but after delving into the below information corresponds to the ITU656 spec:
Sample Rate of 13.5MHz
Resolution : 720x480
Frame Rate: 29.97Hz
Resolution : 720x576
Frame Rate: 25Hz
I hope that helps