Hello All,
I have ported Wilink8 MCP 8.4 driver for twrvf65gs10 platform.
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-VF65GS10
Platform has SDIO multiblock support with DMA. Wl18xx card has been switched to high speed mode ( 50 MHz).
Wl18xx driver has been ported to use Nucleus RTOS.
Currently cortex a5 CPU is running at 396 MHz.
I have measured throughput via iperf on it for Wilink8 driver and the results are as follows:
------------------------------------------------------------
Server listening on TCP port 5001
TCP window size: 256 KByte
------------------------------------------------------------
[ 6] local 0.0.0.0 port 5001 connected with 192.168.0.101 port 53336
[ ID] Interval Transfer Bandwidth
[ 6] 0.0-10.5 sec 8.00 MBytes 6.37 Mbits/sec
------------------------------------------------------------
Client connecting to 192.168.0.100, TCP port 5001
TCP window size: 256 KByte
------------------------------------------------------------
[ 3] local 192.168.0.101 port 50741 connected with 192.168.0.100 port 5001
[ ID] Interval Transfer Bandwidth
[ 3] 0.0-10.1 sec 7.88 MBytes 6.53 Mbits/sec
Is it a reasonable speed? What numbers are expected to get on twrvf65gs10 platform with Wl18xx module? On am335xevm. throughput is very high ( 50 Mbps ) but on vybrid platform, it is very low. Why this is so? Am i missing anything?
已解决! 转到解答。
Hi Amna,
I haven't any experiences with Wilink8, but if you measure throughput, how you was connected? Connection from Vybrid to some router was by wireless LAN and how standard was you use?
If you use standard IEEE 802.11b, is it OK.
If you use standard IEEE 802.11g - question is interferences, number of channel, etc...
Wifi can choose speed by interferences and when looses packets.
Best regards
Vilem
Hello Vilem,
Thanks a lot for your reply.
Yes Connection was by wireless LAN to TP Link Access Point.
I am using IEEE 802.11n standard.
Best Regards
Amna
On Tue, Feb 3, 2015 at 8:26 PM, Vilem Zavodny <admin@community.freescale.com
Hi Vilem,
Yes settings are correct for N standard on module. All the settings are
actually in firmware file which is provided by the vendor so these cannot
be incorrect. Yes, I can choose between different modes.
Thanks
Amna
On Wed, Feb 4, 2015 at 1:18 PM, Vilem Zavodny <admin@community.freescale.com
HI amnawaseem do you have the information requested?