Which CAN Drivers to use for Phytec Vybrid Development Board PCM052 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which CAN Drivers to use for Phytec Vybrid Development Board PCM052 ?

Jump to solution
1,686 Views
swapnilv
Contributor III

Hi,

I am using Phytec Vybrid Development board (PCM052). Kindly let me know whether I should use FlexCAN or SocketCAN Drivers for CAN communication.

Thanks & Regards,

Swapnil Vaychale

Labels (2)
0 Kudos
Reply
1 Solution
1,432 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Swapnil,

They are not exclusive, actually SocketCAN Drivers are implemented to work over FlexCAN. It would be hard to work over the FlexCAN module sending raw data.

Regards,

Carlos

View solution in original post

0 Kudos
Reply
2 Replies
1,433 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Swapnil,

They are not exclusive, actually SocketCAN Drivers are implemented to work over FlexCAN. It would be hard to work over the FlexCAN module sending raw data.

Regards,

Carlos

0 Kudos
Reply
1,432 Views
swapnilv
Contributor III

Thanks for your reply Carlos.

Regards,

Swapnil

0 Kudos
Reply