What is the state of PTA9 after a reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the state of PTA9 after a reset

1,133 Views
richardcopeman
Contributor II

After a reset what is the default function of pin PTA9 on the TWR-VF65GS10 board?

Labels (1)
0 Kudos
Reply
1 Reply

1,026 Views
Yuri
NXP Employee
NXP Employee

Hello,

  According to table in section 12.1 (Pinouts) of the Vybrid Datasheet,

default function of PTA9 is JTDI. 

https://www.nxp.com/docs/en/data-sheet/VYBRIDFSERIESEC.pdf 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply