WDOG of LPSTOP3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

WDOG of LPSTOP3

3,300件の閲覧回数
soichiyamamoto
Contributor V

Hi,

I have a question for WDOG of LPSTOP3.

I hurry very much. Please give me a response early.

Q1)

Does low frequency reference clocks which is a clock source of WDOG stop in LPSTOP3 mode?

Q2)

At the time of LPSTOP3 mode, is there a method not to stop WDOG?

Q3)

In LPSTOP3 mode, does WDOG do LOST?

Best Regards,

soichi

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

1,527件の閲覧回数
naoumgitnik
Senior Contributor V

Dear Soichi,

Regarding the Watchdog low frequency clock sources, please, refer to the "WDOG clocking options" section of the Reference Manual.

Most likely, based on this information, you will derive answers for the rest of the questions.

Sincerely, Naoum Gitnik.

0 件の賞賛
返信

1,527件の閲覧回数
soichiyamamoto
Contributor V

Dear Naoum,

Thank you for reply.

Q1)

Is WDOG PD1? Or is it PD0?

※PD:Power Domain

Q2)

During LPSTOP3 mode, do you do LOST?

Best regards,

soichi

0 件の賞賛
返信

1,527件の閲覧回数
naoumgitnik
Senior Contributor V

Dear Soichi,

  • I will check Q1. If not a secret, what triggered this question, please?
  • Regarding Q2: to expedite the process, may you, please, refer me to our documentation place triggering this question?

Sincerely, Naoum Gitnik.

0 件の賞賛
返信

1,527件の閲覧回数
ShunsukeMatsuno
NXP Employee
NXP Employee

Hi Naoum,

Please let me explain the background of these questions.

Our customer is facing the hang up issue after LPSTOP exiting, which is discussed in the following thread.

(Hand up issue from LPSTOP3 mode)

https://community.freescale.com/message/387150#387150

They have not found the root cause of the issue yet, however their production is near-market. So they are considering WDOG as software workaround. They want to use WDOG to reset system when the hang up issue happens.

We would like to know if WDOG works properly during LPSTOP or not.

Best regards,

Matsuno

0 件の賞賛
返信

1,527件の閲覧回数
soichiyamamoto
Contributor V

Dear Naoum,

I am always grateful for the daily support that you give me.

My application uses LPSTOP3 for intermittent operation.

And I want to use WDOG for time when irregular happened.

The above is the target of the question.

If WDOG does not function in LPSTOP3, I will put WDOG outside.

I am waiting for your response.

Best Regards,

soichi

0 件の賞賛
返信

1,527件の閲覧回数
naoumgitnik
Senior Contributor V

Dear Soichi,

Unfortunately, there is no WDOG in the power domain 0.

Regards, Naoum Gitnik.

ShunsukeMatsuno

0 件の賞賛
返信