Vybrid (vf610) Chip Errata document

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Vybrid (vf610) Chip Errata document

1,818件の閲覧回数
lukaszmajewski
Contributor III

Dear Community,

I would like to ask if there is a "Chip errata" document for Vybrid (e.g. vf610)?

I'm asking since there are some issues with DMA usage with DSPI controller and also QSPI controller HW issues as pointed out in the Linux kernel code:

(What's more is that there is a bug in  the "IP Command Read" in the Vybrid.) found here:
 https://elixir.bootlin.com/linux/v4.19-rc4/source/drivers/mtd/spi-nor/fsl-quadspi.c#L671

I've found some Vybrid errata: https://www.nxp.com/docs/en/errata/VYBRID_2N02G.pdf 

but it seems a bit outdated now. It also doesn't provide information, which I need.

For example - the iMX6Q has a very detailed (and up to date) "Chip Errata" document:

ラベル(3)
タグ(2)
1 返信

1,517件の閲覧回数
lukaszmajewski
Contributor III

Could anybody from NXP comment on this issue?

Thanks in advance,

Łukasz