Vybrid input video signal when flicker noise has occurred.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Vybrid input video signal when flicker noise has occurred.

跳至解决方案
2,320 次查看
takashitakahash
Contributor III

Hi ncommunity.

Our customer has video signal flicker noise issues.

Input video signal to Vibrid When the video signal flicker has occurred.

Although I think that noise cause of the input signal, what  can reduce the noise by setting the register?

Also,  can I determine the effect by monitoring the value of the VDEC_NOISE?

标签 (1)
0 项奖励
回复
1 解答
1,989 次查看
jiri-b36968
NXP Employee
NXP Employee

Hello Takashi-san,

Please rephrase your reply and add some details. 0.22uF works or not?

On reference board is used 0.1uF.

pastedImage_0.png

/Jiri

在原帖中查看解决方案

9 回复数
1,989 次查看
takashitakahash
Contributor III

Hellow Karina-san.

Customer  has been improved that noise issues showed that with a 0.22μF input coupling capacity.

The recommended value of the Vybrid reference board is 0.022μF.

It is not a problem even with a 0.22μF.

Input is the NTSC signal from the camera.

0 项奖励
回复
1,990 次查看
jiri-b36968
NXP Employee
NXP Employee

Hello Takashi-san,

Please rephrase your reply and add some details. 0.22uF works or not?

On reference board is used 0.1uF.

pastedImage_0.png

/Jiri

1,989 次查看
takashitakahash
Contributor III

Customer using Integlity of GHS OS.

Hard ware is there own board.

Video signal is analog NTSC, it converting the built-in ADC to  the digital signal.

Symptoms is not a frame flicker, noise level (SN ratio) large, and  visible as noise is flickering.

0 项奖励
回复
1,989 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

jiri-b36968​ can you continue with the follow up?

0 项奖励
回复
1,989 次查看
jiri-b36968
NXP Employee
NXP Employee

Hello Takashi-san,

Is the problem in video input signal or setting of the display is not correct?

Please add some details: Video of the issue, setting of VideoADC, parameters of the input signal and the noise, configuration of Vybrid, etc.

/Jiri

0 项奖励
回复
1,989 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

takashitakahashi​ did you get previous comment?

0 项奖励
回复
1,989 次查看
timesyssupport
Senior Contributor II

Hello Takashi,

Can you describe your customer's hardware and OS configuration?

Is this a Vybrid VF5xx based design? Is Linux running on this hardware, or another OS?

How is the video signal input connected to the hardware?

Thank you,

Timesys Support

0 项奖励
回复
1,989 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

takashitakahashi​ did you get previous comment?

0 项奖励
回复
1,989 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you attend this case?

0 项奖励
回复