Vybrid and LVDS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Vybrid and LVDS

跳至解决方案
1,188 次查看
jimma
Contributor I

Hi,

I am working with a TWR VF65GS10 and I would like to connect an ADC with LVDS output to the Vybird,

I'm quite new to high speed ADCs and DACs, so I'm not familiar with how these devices are connected.

I've read the VybridRM but didn't found a lot of information, is there an app note, example or maybe someone have some more information, is this application possible and if yes where can I find more information about it ?

Regards,

Jim.

标签 (2)
标记 (5)
0 项奖励
回复
1 解答
944 次查看
naoumgitnik
Senior Contributor V

Hello Jim,


It looks like there is no problem with the "Video Interface like the VIU3 on the Vybrid", right? Thus, let's focus on the "would like to connect an ADC with LVDS output to the Vybird" one. - Formally speaking, you have a peripheral with an LVDS interface that you would like to connect to Vybrid.


Unfortunately, Vybrid only has one LVDS pair of pins (LVDS0) and uses it for clock only, so you will have to convert the peripheral's LVDS interface into the single-ended one of a kind that Vybrid accepts (or simply switch to an ADC with the interface type Vybrid supports...).


Sincerely yours, Naoum Gitnik.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
944 次查看
Nouchi
Senior Contributor II

Hello,

Take a look at Quartz board, there's a LVDS interface on it.


Emmanuel

0 项奖励
回复
944 次查看
jimma
Contributor I

Hello Emmanuel,

I think I've already seen this board before, I don't remember exactly why it didn't corresponds to my needs,

I also need a Video Interface like the VIU3 on the Vybrid.

Jim.

0 项奖励
回复
945 次查看
naoumgitnik
Senior Contributor V

Hello Jim,


It looks like there is no problem with the "Video Interface like the VIU3 on the Vybrid", right? Thus, let's focus on the "would like to connect an ADC with LVDS output to the Vybird" one. - Formally speaking, you have a peripheral with an LVDS interface that you would like to connect to Vybrid.


Unfortunately, Vybrid only has one LVDS pair of pins (LVDS0) and uses it for clock only, so you will have to convert the peripheral's LVDS interface into the single-ended one of a kind that Vybrid accepts (or simply switch to an ADC with the interface type Vybrid supports...).


Sincerely yours, Naoum Gitnik.

0 项奖励
回复
944 次查看
Nouchi
Senior Contributor II

Hello Jim,

Their board use a  SN75LVDS84A to convert RGB into LVDS.

Look at TI, there's many LVDS lines driver and SERDES.

What do you plan to do exactly ?

0 项奖励
回复