Hi,
according to the reference manual, the UART0/UART1 include features like Initial Charachter Detection, Transmit Threshold detection and so on. But in chapter 49 (UART) of the RM, these features are not described and only registers used by all UARTs are listed. Is there a detailed manual about these features or simply a short description about the missing registers?
Thanks in advance
Solved! Go to Solution.
Hi,
As I see, those features are related to the ISO 7816 smartcard support and more information regarding this feature can be found at chapter 49.4.7 ISO-7816/smartcard support. Have you checked that part?
/Alejandro
mathiaswaldenburger did you get previous comment?