Vybrid VF6xx, Flex Timer, FAULT input

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vybrid VF6xx, Flex Timer, FAULT input

Jump to solution
2,625 Views
axelrichter
Contributor I

Hello!

we want to use the Flextimer of the Vybrid as a H Bridge driver together with a FAULT input to set the output in a safe state.

In reference manual it is described how to initialize the FAULT input but not mentioned which input pin is used for it.

Is there a dedicated pin for that? So which pin is it?

Or can I use any other pin? How and where can I configure it in this case?

Best regards,

Axel Richter

Labels (2)
0 Kudos
Reply
1 Solution
2,452 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
3 Replies
2,453 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
2,453 Views
axelrichter
Contributor I

Any GPIO can be used, when configured as interrupt input. In the interrupt handling routine the desired fault bit in SRC_MISC1 has to be set.

0 Kudos
Reply
2,453 Views
richard_stulens
NXP Employee
NXP Employee

That is indeed correct.

Regards,

Richard

0 Kudos
Reply