Vybrid VF6xx, Flex Timer, FAULT input

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Vybrid VF6xx, Flex Timer, FAULT input

ソリューションへジャンプ
1,717件の閲覧回数
axelrichter
Contributor I

Hello!

we want to use the Flextimer of the Vybrid as a H Bridge driver together with a FAULT input to set the output in a safe state.

In reference manual it is described how to initialize the FAULT input but not mentioned which input pin is used for it.

Is there a dedicated pin for that? So which pin is it?

Or can I use any other pin? How and where can I configure it in this case?

Best regards,

Axel Richter

ラベル(2)
0 件の賞賛
1 解決策
1,544件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
3 返答(返信)
1,545件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
1,545件の閲覧回数
axelrichter
Contributor I

Any GPIO can be used, when configured as interrupt input. In the interrupt handling routine the desired fault bit in SRC_MISC1 has to be set.

0 件の賞賛
1,545件の閲覧回数
richard_stulens
NXP Employee
NXP Employee

That is indeed correct.

Regards,

Richard

0 件の賞賛